Skip to main content
julien
Associate III
April 17, 2008
Question

SOLVED : USART_SendData

  • April 17, 2008
  • 9 replies
  • 1984 views
Posted on April 17, 2008 at 11:24

SOLVED : USART_SendData

    This topic has been closed for replies.

    9 replies

    julien
    julienAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    Hello,

    I'm using USART_SendData function, and i'm surprised that when i transmit the value ''224''(decimal) i receive ''248''.

    USART_SendData(USART1, 224);

    or if I transmit ''65'' I receive ''224''..

    my configuration :

    USART_InitStructure.USART_BaudRate = 9600;

    USART_InitStructure.USART_WordLength = USART_WordLength_8b;

    USART_InitStructure.USART_StopBits = USART_StopBits_1;

    USART_InitStructure.USART_Parity = USART_Parity_No;

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

    USART_InitStructure.USART_Clock = USART_Clock_Disable;

    USART_InitStructure.USART_CPOL = USART_CPOL_Low;

    USART_InitStructure.USART_CPHA = USART_CPHA_2Edge;

    USART_InitStructure.USART_LastBit = USART_LastBit_Disable;

    /* Configure the USART1 */

    USART_Init(USART1, &USART_InitStructure);

    USART_Cmd(USART1, ENABLE);

    I don't understand ..

    thanks

    [ This message was edited by: julien.massot on 15-04-2008 15:43 ]

    [ This message was edited by: julien.massot on 17-04-2008 14:54 ]

    julien
    julienAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    My host Uart is the USART1, I'm using the firmware library um0427

    GPIO :

    /* Configure USART1 Tx as alternate function push-pull */

    GPIO_InitStructureU.GPIO_Pin = GPIO_Pin_9;

    GPIO_InitStructureU.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructureU.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_Init(GPIOA, &GPIO_InitStructureU);

    /* Configure USART1 Rx (PD.10) as input floating */

    GPIO_InitStructureU.GPIO_Pin = GPIO_Pin_10;

    GPIO_InitStructureU.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_Init(GPIOA, &GPIO_InitStructureU);

    On my PC i launch a sniffer who reads the decimal value

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    What is your host UART or other part configuration ?

    julien
    julienAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    Com6

    baud 9600

    Data 8

    Parity none

    Stop 1

    However

    this function works properly, and return the good value

    do

    {

    if((USART_GetFlagStatus(USART1, USART_FLAG_RXNE) != RESET)&&(RxCounter < RxBufferSize))

    {

    RxBuffer[RxCounter] = USART_ReceiveData(USART1);

    USART_SendData(USART1, RxBuffer[RxCounter++]);

    }

    }while(RxCounter != RxBufferSize);

    strange..

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    Bonjour Julien,

    I mean what is the full configuration of the PC sniffer ?

    baudrate, partity, etc.. thank you.

    Cheers,

    STOne-32.

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    Hi Julien,

    lanchon suggestion is right and you should modifiy in the file called

    ''stm32f10x_conf.h''

    Just before the Assert macro

    /* In the following line adjust the value of External High Speed oscillator (HSE)

    used in your application */

    #define HSE_Value ((u32)8000000) /* Value of the External oscillator in Hz*/

    By #define HSE_Value ((u32)12000000) /* Value of the External oscillator in Hz*/

    Hope this is more clear now. Cheers,

    STOne-32.

    julien
    julienAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    Thanks,

    I'm using an external crystal at 12Mhz, PLL factor is configure at 6 :

    RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_6);

    So i'm running at 72 Mhz..

    I'm searching with gdb..

    lanchon
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    hi,

    I don't know the USART peripheral, but couldn't help but notice that

    224 = 0xE0 = 11100000

    248 = 0xF8 = 11111000

    it smells like maybe there's a significant difference (40%) in baud rate between transmitter and receiver. check your clock frequency. I assume you're using a crystal, the firmware lib expects the frequency of the external crystal in a #define directive. the default is 8MHz.

    julien
    julienAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:30

    Thank you STOne and good suggestion Lanchon..

    Now my Usart works properly...