Associate II
June 15, 2015
Question
[solved] STM32L151UC: SPI3 problem - no activity on pins
- June 15, 2015
- 1 reply
- 565 views
Posted on June 15, 2015 at 14:20
Hello,
I am trying to configure the SPI3 port of an STM32L151UC micro controller. I have tried several things but I see no output on the related pins. When using gpios instead of the AF of the SPI peripheral, I can control the pins and therefore verify that the hardware connections are ok. I would be satisfied to see the pins toggling, under any CPOL, speed, NSS, etc configuration. I have narrowed my tests down to a simple hello project as produced by the latest Eclipse version with GNU Cross Arm Gcc toolchain, adding only the peripheral drivers and device.h info. My debugger is J-Link pro, not that I think this matters. An example code that reproduces the problem is:void spi_conf(void){ GPIO_InitTypeDef GPIO_InitStructure; SPI_InitTypeDef SPI_InitStructure; RCC->APB1ENR = 0xffffffff; RCC->APB2ENR = 0xffffffff; RCC->AHBENR = 0xffffffff; RCC->APB1LPENR = 0xffffffff; RCC->APB2LPENR = 0xffffffff; RCC->AHBLPENR = 0xffffffff; //Or alternatively: //RCC_APB2PeriphClockCmd ( RCC_APB2Periph_SYSCFG, ENABLE); //RCC_APB1PeriphClockCmd ( RCC_APB1Periph_SPI3, ENABLE); //RCC_AHBPeriphClockCmd ( RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB | RCC_AHBPeriph_GPIOC, ENABLE); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI3, &SPI_InitStructure); SPI_Cmd(SPI3, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_PinAFConfig(GPIOC,GPIO_Pin_10,GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC,GPIO_Pin_11,GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC,GPIO_Pin_12,GPIO_AF_SPI3); GPIO_Init(GPIOC, &GPIO_InitStructure); while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_TXE) == RESET) ; } And then main.c calls this function followed by SPI_I2S_SendData (SPI3, 0xa5); int SPI3val=SPI_I2S_ReceiveData(SPI3); in a loop. But I see no activity in the HCLK or HMOSI. They do not go high even when I change the CPOL. The oscilloscope is '100MHz' so I would expect at least something. When I tried to poll the BSY, I saw that it takes some iterations until it is cleared, which would indicate that the peripheral is active. Am I missing some configuration? I use the HSI clock, would I reach this point if something on the _initialize_hardware.c went wrong? Grateful for any hint Edit: Attached sample project including its compiled output #spi #stm32l151