Skip to main content
Just Matt
Associate III
January 3, 2014
Question

Solved: STM32F4Discovery EXTI Multiple Interrupts

Posted on January 03, 2014 at 03:17

EDIT: Solved by clive1! See post below.

Hi (again), I'm tinkering with Interrupts this week. I'n the example code I have provided below, The Green light flashes (as expected) in the loop. The EXTI0 fires when I bring the PA0 pin high. However, when I bring the PC5 pin high nothing happens :( Not sure, what i'm doing wrong, or is there a special way of handeling multiple interrupts? Google and the (soso) search here didn't show much. As always any help is appreciated!

#include <stm32f4xx_gpio.h>
#include <stm32f4xx_rcc.h>
#include <stm32f4xx_exti.h>
#include <stm32f4xx_syscfg.h>
#include <stm32f4xx.h>
#include <misc.h>
void
InitGPIO(GPIO_TypeDef*, uint16_t, GPIOMode_TypeDef);
void
Attach_GPIO_Interrupt(uint8_t, uint8_t, uint32_t, EXTITrigger_TypeDef, uint8_t);
void
Delay();
int
main()
{
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
InitGPIO(GPIOA, GPIO_Pin_0, GPIO_Mode_IN); 
//initialise PA0 is input
InitGPIO(GPIOC, GPIO_Pin_5, GPIO_Mode_IN);
// PC5 as input
//Green
InitGPIO(GPIOD, GPIO_Pin_12, GPIO_Mode_OUT);
//Blue
InitGPIO(GPIOD, GPIO_Pin_15, GPIO_Mode_OUT);
//Orange
InitGPIO(GPIOD, GPIO_Pin_13, GPIO_Mode_OUT);
//attach interrupt to GPIO PA0
Attach_GPIO_Interrupt(EXTI_PortSourceGPIOA, EXTI_PinSource0, EXTI_Line0, EXTI_Trigger_Rising, 1);
//interrupt to PC5
Attach_GPIO_Interrupt(EXTI_PortSourceGPIOC, EXTI_PinSource5, EXTI_Line2, EXTI_Trigger_Rising_Falling, 1);
for
(;;)
{
GPIO_WriteBit(GPIOD, GPIO_Pin_12, Bit_SET);
Delay();
GPIO_WriteBit(GPIOD, GPIO_Pin_12, Bit_RESET);
Delay();
}
}
extern
''C''
void
EXTI0_IRQHandler(
void
) 
//EXTI0 ISR
{
if
(EXTI_GetITStatus(EXTI_Line0) != RESET) 
//check if EXTI line is asserted
{
EXTI_ClearFlag(EXTI_Line0); 
//clear interrupt
//Enter your code here
GPIO_WriteBit(GPIOD, GPIO_Pin_15, Bit_SET);
Delay();
GPIO_WriteBit(GPIOD, GPIO_Pin_15, Bit_RESET);
}
}
extern
''C''
void
EXTI2_IRQHandler(
void
) 
//EXTI2 ISR
{
if
(EXTI_GetITStatus(EXTI_Line2) != RESET) 
//check if EXTI line is asserted
{
EXTI_ClearFlag(EXTI_Line2); 
//clear interrupt
//Enter your code here
GPIO_WriteBit(GPIOD, GPIO_Pin_13, Bit_SET);
Delay();
GPIO_WriteBit(GPIOD, GPIO_Pin_13, Bit_RESET);
}
}
void
Delay()
{
int
i;
for
(i = 0; i < 1000000; i++)
asm(
''nop''
);
}
void
InitGPIO(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin, GPIOMode_TypeDef GPIO_Mode)
{
GPIOPuPd_TypeDef PuPdMode = GPIO_PuPd_NOPULL;
GPIO_InitTypeDef GPIO_InitStructure;
switch
(GPIO_Mode)
{
case
GPIO_Mode_OUT:
PuPdMode = GPIO_PuPd_NOPULL; 
//digital output. Not using open drain mode as I do not know how that operates
break
;
case
GPIO_Mode_IN:
PuPdMode = GPIO_PuPd_NOPULL; 
//digital read have Pin as input floating
break
;
case
GPIO_Mode_AN:
PuPdMode = GPIO_PuPd_NOPULL; 
//for analogue read have Pin as input floating
break
;
case
GPIO_Mode_AF: 
//need to do a remapping if using alternate functions
PuPdMode = GPIO_PuPd_UP; 
//for PWM have not looked at accounting for the various other alternate functions
break
;
}
GPIO_InitStructure.GPIO_Pin = GPIO_Pin;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode;
//GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; //used for digital output and PWM output
//this setting does not matter for ADC and digital read
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz;
GPIO_InitStructure.GPIO_PuPd = PuPdMode;
GPIO_Init(GPIOx, &GPIO_InitStructure);
}
void
Attach_GPIO_Interrupt(uint8_t EXTI_PortSourceGPIOx, uint8_t EXTI_PinSourcex, uint32_t EXTI_Line,
EXTITrigger_TypeDef EXTI_Trigger, uint8_t Priority)
{
uint8_t EXTI_IRQn = 0;
switch
(EXTI_Line)
{
case
0x1:
EXTI_IRQn = EXTI0_IRQn;
break
;
case
0x2:
EXTI_IRQn = EXTI1_IRQn;
break
;
case
0x4:
EXTI_IRQn = EXTI2_IRQn;
break
;
case
0x8:
EXTI_IRQn = EXTI3_IRQn;
break
;
case
0x10:
EXTI_IRQn = EXTI4_IRQn;
break
;
case
0x20: 
case
0x40: 
case
0x80: 
case
0x100: 
case
0x200:
EXTI_IRQn = EXTI9_5_IRQn;
break
;
case
0x400: 
case
0x800: 
case
0x1000: 
case
0x2000: 
case
0x4000: 
case
0x8000:
EXTI_IRQn = EXTI15_10_IRQn;
break
;
}
/* Connect EXTI Line to appropriate GPIO Pin */
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOx, EXTI_PinSourcex);
NVIC_InitTypeDef NVIC_InitStructure;
EXTI_InitTypeDef EXTI_InitStructure;
/* Configure EXTI Line */
EXTI_InitStructure.EXTI_Line = EXTI_Line;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
/* Enable and set EXTI Line Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = EXTI_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = Priority;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x01;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    January 3, 2014
    Posted on January 03, 2014 at 03:57

    Pin 5 would be Exti line 5, into EXTI9_5_IRQHandler

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Just Matt
    Just MattAuthor
    Associate III
    January 3, 2014
    Posted on January 03, 2014 at 04:26

    Once again, Thanks Clive1! 

    12.2.2 of the Reference Manual completely missed it >_<

    -Matt