Skip to main content
DavidAlfa
Senior II
April 13, 2022
Solved

[SOLVED] SCK idling high when SPI module is stopped

 FIX: Enable pull-down resistor in SCK pin

Init parameters:

  • CPOL=0 CPHA =0, so SCK level should be idling at LOW level.
  • Software NSS
  • Half-Duplex, master mode

Software: CubeIDE 1.9, CubeMX 6.5.0

Device: STM32F411CE

Issue:

  • Regardless of the clock config, SCK is high if the SPI module is disabled.
  • When enabling CS before calling HAL_SPI_Transmit/Receive, the slave sees SCK high, breaking the transfer.
  • After a Transmit, the SPI module is left enabled, holding SCK low, so next transfer will work.
  • After a Receive, SPI module is disabled, breaking SCK again.

The issue can be seen here:

0693W00000LxuCUQAZ.png

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
April 13, 2022

When you disable SPI (by clearing SPE bit), SCK is threestated. If it goes up, it's because there is a pullup, internal or external.

If you don't like Cube/HAL's behaviour, simply don't use it. SPI is simple enough to be used normally.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
April 13, 2022

When you disable SPI (by clearing SPE bit), SCK is threestated. If it goes up, it's because there is a pullup, internal or external.

If you don't like Cube/HAL's behaviour, simply don't use it. SPI is simple enough to be used normally.

JW

DavidAlfa
DavidAlfaAuthor
Senior II
April 13, 2022

Enabling the pulldown resistor fixed the clock idle issue, Thanks!