Skip to main content
DJ001
Associate II
January 5, 2023
Solved

Solution architecture help

I need help in implementing a solution. I'd like to implement a system that measures elapsed time (ET) between two digital input (DI) pulses. These two signals will be on different channels. There are 4 sets of signal, therefore I need to measure four things: ET(0) = DI(0) -> DI(1), ET(1) = DI(2) -> DI(3), ET(2) = DI(4) -> DI(5), ET(4) = DI(6) -> DI(7).

The counting should be between positive edges, resolution should be in microseconds, maximum time will be <= 2s. Each of the measurements should reset on DI(x) and store on DI(x+1). It is possible that multiple DI(x) will occur before DI(x+1) therefore ET will always be the measurement between DI(x+1) and the last DI(X)

I first implemented a solution with a raspberry pi pico. That solution implemented an interrupt on each of the digital input channels that triggered on a positive transition. The interrupt handler essentially queues up the DI index and a 64bit microsecond tick count on a pre initialized queue. The super loop monitors the queue and figures out the elapsed times based on what comes through the queue.

For a number of reasons it's desirable to move to the STM32 foamily. In this case the L432KC was selected because of its form factor and its inclusion of a CAN peripheral.

Could someone offer any suggestions no how to approach this problem with the L432KC? Additionally, I'd be willing to move to a different family member if there is a compelling reason.

Thanks for the help

This topic has been closed for replies.
DJ001
DJ001Best answer
Associate II
January 7, 2023

Thanks for the note on this. I obviously have more reading to do. I've come across "AN4776 General-purpose timer cookbook for STM32 microcontrollers" that hopefully will help me wrap my head around the various options

6 replies

gbm
Super User
January 5, 2023

Two 4-channel timers, possibly synchronized, capture mode. If you really need 32-bit resolution, use TIM2 and TIM5.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
DJ001
DJ001Author
Associate II
January 5, 2023

Thanks for the clue. This is great! The capture mode functionality seems to be what I'm after. Now I know where to focus my studies... Looks like we'll need to move up to a NUCLEO-G474RE to get the timers and CAN.

S.Ma
Principal
January 7, 2023

Also take note that some chips have a dma which can store capture valuee in a ram buffer, if you like to reduce interrupt frequency. A bit more advanced.

DJ001
DJ001AuthorBest answer
Associate II
January 7, 2023

Thanks for the note on this. I obviously have more reading to do. I've come across "AN4776 General-purpose timer cookbook for STM32 microcontrollers" that hopefully will help me wrap my head around the various options

Piranha
Principal III
January 7, 2023

F3, H7 and G4 series also have a HRTIM peripheral with a plenty of timer instances. Though, if I'm not mistaken, those timers are 16-bit and therefore the software would have to count the overflows. Anyway, AN4539 provides more information about it.

DJ001
DJ001Author
Associate II
January 7, 2023

Thank you