Skip to main content
brj
Associate III
Nov 27, 2008 6:28 AM UTC
Question

Software reset on STM32

Posted on November 27, 2008 at 07:28

Software reset on STM32

    This topic has been closed for replies.

    5 replies

    joseph239955
    Visitor II
    May 17, 2011 10:23 AM UTC
    Posted on May 17, 2011 at 12:23

    Hi Brian,

    If you only want to reset the Cortex-M3, you can use a register in the NVIC called Application Interrupt and Reset Control register (Address 0xE000ED0C), bit 0 (VECTRESET).

    It might be easier to see what went wrong if you can tell us the value of fault status registers and if possibly, dis-assembled code generated by the compiler.

    brj
    brjAuthor
    Associate III
    May 17, 2011 10:23 AM UTC
    Posted on May 17, 2011 at 12:23

    Hi all,

    I am trying to perform a software reset of a program runing in flash, but it ends up in the HardFaultExecption handler.

    I did copy a code snippet from an IAP application note:

    typedef void (*pFunction)(void);

    pFunction Jump_To_Application;

    #define ApplicationAddress 0x8000000

    /**

    * @brief Executes a jump to code memory start adr. Soft reset.

    * @param None

    * @return Nothing

    */

    void ResetAppl(void)

    {

    u32 JumpAddress;

    JumpAddress = *(vu32*) (ApplicationAddress + 4);

    /* Jump to user application */

    Jump_To_Application = (pFunction) JumpAddress;

    /* Initialize user application's Stack Pointer */

    __MSR_MSP(*(vu32*) ApplicationAddress);

    Jump_To_Application();

    }

    When debugging I can see that the function pointer points to 0x080046E1 ??

    Why ? shouldent it point to 0x08000004 ? however modifying the address to 0x08000004 doesent help either !

    btw. I use the IAR ARM 5.11 compiler.

    Best regards

    Brian

    trevor1
    Associate III
    May 17, 2011 10:23 AM UTC
    Posted on May 17, 2011 at 12:23

    See NVIC_GenerateSystemReset function in the ST firmware library. If your using the firmware library just call this function.

    niek_ebbers
    Associate II
    May 17, 2011 10:23 AM UTC
    Posted on May 17, 2011 at 12:23

    [ This message was edited by: niek_ebbers on 27-11-2008 11:12 ]

    niek_ebbers
    Associate II
    May 17, 2011 10:23 AM UTC
    Posted on May 17, 2011 at 12:23

    Not using the firmware. I like a good challenge :)

    But it worked perfectly. In my case:

    Scb.AIRCR.all = 0x05FA0000 | (u32)0x04;

    Thanks!