Skip to main content
S.Kamath
Associate III
February 18, 2023
Solved

Software migration from STM32F207IGH (Cortex-M3) to STM32F427IIH6 (Cortex-M4)

STM32F207IGH used in the existing product. We see that we need more Flash & SRAM to include more software features. STM32F427II is having double the size of both Flash & SRAM. What is the process to migrate software to STM32F427II? Micrium RTOS used in the existing product. Is there any easy way to migrate software code?

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
February 18, 2023

I have no personal experience with such migration, but unless the RTOS or any other tool you are using gets into way, the migration should be very straighforward as the 'F407/'F427 are a direct update of the 'F207 - almost everything is identical or better.

I am aware of one notable exception, and that is the value of divider of VBAT measurement in ADC and also numbers of VBAT/VREF channels in ADC, but that is a minor issue.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
February 18, 2023

I have no personal experience with such migration, but unless the RTOS or any other tool you are using gets into way, the migration should be very straighforward as the 'F407/'F427 are a direct update of the 'F207 - almost everything is identical or better.

I am aware of one notable exception, and that is the value of divider of VBAT measurement in ADC and also numbers of VBAT/VREF channels in ADC, but that is a minor issue.

JW

S.Kamath
S.KamathAuthor
Associate III
February 20, 2023

Thanks JW, This helps!