Skip to main content
z1060
Associate II
September 30, 2016
Question

Software interrupt doesn't work

Posted on September 30, 2016 at 13:41

Hello!

I use STM32F429ZI and I try to set a software interrupt, but it doesn't work.

I set it as follows:

    EXTI->IMR |= EXTI_IMR_MR0;

 

    NVIC_SetPriority(EXTI0_IRQn, 15);

 

    NVIC_EnableIRQ(EXTI0_IRQn);

 

    

 

   

 

    __HAL_GPIO_EXTI_GENERATE_SWIT(EXTI_SWIER_SWIER0);

 

 

void EXTI0_IRQHandler (void)

 

{

 

    SET(TEST_X2);//test point

 

}

 

 

Software interrupt is not trigered. Help me please. Am I missing something?

Thank you for your help.

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    September 30, 2016
    Posted on September 30, 2016 at 15:13

    SYSCFG clock enabled?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    slimen
    Visitor II
    September 30, 2016
    Posted on September 30, 2016 at 15:35

    Hello,

    Make sure you've configured the pins, and that the GPIO and SYSCFG clocks are enabled.

    Regards

    z1060
    z1060Author
    Associate II
    September 30, 2016
    Posted on September 30, 2016 at 15:38

    Yes, I use __HAL_RCC_SYSCFG_CLK_ENABLE(); in HAL_GPIO_Init