Skip to main content
Associate
January 2, 2024
Question

SMT32F407VGT6 / CAN issue

  • January 2, 2024
  • 1 reply
  • 788 views

The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!

1 reply

Tesla DeLorean
Guru
January 2, 2024

Check performance of external clock and transceiver. 

You can output HSE via PA8 (MCO) and check clock accuracy within specification limits. 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..