Skip to main content
Associate
May 22, 2024
Solved

SMBus on STM32C031

Hi ST tesam,

When I use  HAL_SMBUS_Master_Receive_IT( ) to receive data from device ,I can not got the information directly after the HAL_SMBUS_MasterRxCpltCallback( SMBUS_HandleTypeDef *hsmbus ) was complete.

(I had set a flag when HAL_SMBUS_MasterRxCpltCallback( SMBUS_HandleTypeDef *hsmbus )  done)

I had to wait for a while and then I can read data from register, but what can I do to know when the saving process was complete?

 

Regards,

LSN

This topic has been closed for replies.
Saket_OmBest answer
ST Technical Moderator
May 27, 2024

Hello @LsnLeeJW 

 

Could you please try to check the state in the SMBUS handle instead of checking bSMBusRxCpltFlag flag? 

Please refer to the snippet code below to implement this solution: 

 

 
HAL_SMBUS_Master_Receive_IT( &hsmbus1, BATTERY_ADD, &ucCalTemp[ 3 ], dataLength + 1 , SMBUS_LAST_FRAME_NO_PEC );
while (hsmbus1.State == HAL_SMBUS_STATE_MASTER_BUSY_RX);

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

4 replies

ST Technical Moderator
May 22, 2024

Hello @LsnLeeJW and welcome to the community

Could you please provide the source code for this implementation?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
LsnLeeJWAuthor
Associate
May 27, 2024

Hello,Omar.

Thank for your reply,I've attached the snippet of the code.

Here I try to use 'HAL_SMBUS_MasterRxCpltCallback' to notify me whether the data was received,but it don't works.Is there a better way for me to know whether the data has been stored in memory?

Saket_OmBest answer
ST Technical Moderator
May 27, 2024

Hello @LsnLeeJW 

 

Could you please try to check the state in the SMBUS handle instead of checking bSMBusRxCpltFlag flag? 

Please refer to the snippet code below to implement this solution: 

 

 
HAL_SMBUS_Master_Receive_IT( &hsmbus1, BATTERY_ADD, &ucCalTemp[ 3 ], dataLength + 1 , SMBUS_LAST_FRAME_NO_PEC );
while (hsmbus1.State == HAL_SMBUS_STATE_MASTER_BUSY_RX);

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om