Skip to main content
Nnabb.1
Associate II
March 28, 2024
Solved

size of flash in STM32G0J6

Spoiler
 

Hi, 

I have a question about the size of the flash of STM32G0J6. When i use STM32 cube programmer - CLI i saw that the size of the flash of the STM32G0J6 is 64Kb. I try to write everywhere in this memory it works. The datasheet say that the STM32G0J6 flash size is 32Kb and when you look at register 0x1FFFF75E0 it says that the flash size is 32Kb. Is it  normal ? 

 

This topic has been closed for replies.
Nnabb.1
Nnabb.1Best answer
Associate II
April 15, 2024

conclusion : 

STM32G031J6 have a 64kb of usable flash

register 0x1FFFF75E0 return 32Kb 

Datasheet says it has only 32Kb of flash 

If you want to read protect the flash you have enough bit to protect 64Kb ( and you have to set all these bit ). 

I will check other models of microcontroller if we have the same problem. 

7 replies

Nnabb.1
Nnabb.1Author
Associate II
March 28, 2024

it is the STM32G031J6

ST Technical Moderator
March 28, 2024

Hello @Nnabb.1 ,

Which CubeProgrammer version are you using?

Flash size information in Datasheet for STM32G031J6 is (32KB). 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Nnabb.1
Nnabb.1Author
Associate II
March 28, 2024

hi , 

I use STM32CubeProgrammer v2.13.1. But know i have my forth core that use more than 32Kb. It works perfectly on it. 

Nnabb.1
Nnabb.1AuthorBest answer
Associate II
April 15, 2024

conclusion : 

STM32G031J6 have a 64kb of usable flash

register 0x1FFFF75E0 return 32Kb 

Datasheet says it has only 32Kb of flash 

If you want to read protect the flash you have enough bit to protect 64Kb ( and you have to set all these bit ). 

I will check other models of microcontroller if we have the same problem. 

Tesla DeLorean
Guru
April 15, 2024

One die frequently services several part# and an appropriate subset of the FLASH is tested at Final Test

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Nnabb.1
Nnabb.1Author
Associate II
April 16, 2024

Ok but you still have a problem with the documentation. To write protect the flash you have to consider that you have 64Kb of flash and not 32Kb in FLASH_WRP. If you don't set all the bit it doesn't works.