Skip to main content
YANG ERTF
Visitor II
August 25, 2017
Question

Simulink error, STM32-MAT package, Function call from timer interrupt

  • August 25, 2017
  • 3 replies
  • 1135 views
Posted on August 25, 2017 at 10:09

I am following the tutorial that comes with the STM32-MAT package that deals with setting a basic block diagram to run on an STM32 target. In the simulink system I have used the predefined STM32 timer block and set it up at a frequency of 1Hz and to output an interrupt (UP) every second. The output of this block (IRQ UP) is fed as the trigger for a function call block in which I simply toggle a GPIO pin (again with the predefined STM32 GPIO_WRITE block provided in the package).

I have my code generation set to stmtlc and simulation type to 'normal'. I have set up the STMioc file with the necessary timers, interrupts and gpio ports. When I run the simulation I get an error:

An error occurred while running the simulation and the simulation was terminated Caused by: Function-call initiator 'untitled/Timers' attempted to reenable function-call subsystem 'untitled/Function-Call Subsystem' on time step '0.0'. The function-call subsystem cannot be reactivated by the same function-call initiator; there is a flaw in the implementation of the function-call initiator.

I dont understand what the issue is here.

    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    August 28, 2017
    Posted on August 28, 2017 at 13:09

    Hi 

     

    Please precise which tools version are you using ?

    Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Bui Tuan
    Associate
    March 24, 2018
    Posted on March 24, 2018 at 07:33

    I have the same problem. Does anyone have a solution?

    Vinny Vinny
    Visitor II
    May 8, 2018
    Posted on May 08, 2018 at 21:28

    I have the same problem. Does anyone have a solution?