Skip to main content
k_hraj
Associate
October 15, 2011
Question

Simulation Problem in keil 4.2V

  • October 15, 2011
  • 3 replies
  • 970 views
Posted on October 15, 2011 at 10:03

I could not simulate my code written for STM32F205ZE using keil 4.2V.Following is error code it is showing, when I start debug session.

*** error 65: access violation at 0x0000000C : no 'read' permission

If I try to run it is showing:

*** error 65: access violation at 0x00000000 : no 'execute/read' permission

Please give me suggestions to solve this problem.
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    October 15, 2011
    Posted on October 15, 2011 at 17:53

    Please give me suggestions to solve this problem.

     

    http://www.keil.com/support/docs/814.htm

    Try reviewing documentation

    Try Keil technical support

    Try using the most current release (v4.22 last I checked)
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    rales
    Visitor II
    May 31, 2012
    Posted on May 31, 2012 at 16:51

    I have the same problem, and cost about 6 hours screwing around ''trying'' stuff, still doesn't work...

    Never had a problem with NXP,  now I will be ''trying'' a different line of processors!

    Tesla DeLorean
    Guru
    May 31, 2012
    Posted on May 31, 2012 at 17:19

    But ST isn't responsible for the failings of KEIL software.

    KEIL does not represent that the part is simulated.

    http://www.keil.com/dd/chip/5110.htm

    ST has eval boards in the $10-20 range that permit testing on a physical part. Simulators classically fail to represent the nuances of the silicon implementation accurately.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..