Question
simple input routine not working
Posted on November 10, 2011 at 07:35
the ctrl registers remain at reset values but idr 0 an 1 goto low(0). is there something wrong with my source?
// // // //STM32 BUTTON TEST //by T. Herring tre2020067@gmail.com // //////////////////////////////////////////////////////////// //////////////////////////////////////////////////////////// //INCLUDE FILES //these file should already be include in project space and do not need to be //defined again. ////////////////////////////////////////////////////////////// /* #include stm32f10x_vector.c #include stm32f10x_conf.h #include stm32f10x_it.c #include stm32f10x_lib.c */ #include ''stm32f10x_lib.h'' //////////////////////////////////////////////////////////// //FUNCTION PROTOTYPES //////////////////////////////////////////////////////////// //void clockconfig(); void gpio_flash(); void Clk_Init (void) { //RESET CLOCK CONFIG RCC_DeInit(); // 1. Clocking the controller from internal HSI RC (8 MHz) // RCC_HSICmd(ENABLE); // wait until the HSI is ready //while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET); //RCC_SYSCLKConfig(RCC_SYSCLKSource_HSI); // 2. Enable ext. high frequency OSC RCC_HSEConfig(RCC_HSE_ON); // wait until the HSE is ready while(RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET); // 2-1. Set system clock dividers #ifdef EMB_FLASH // 5. Init Embedded Flash // Zero wait state, if 0 < HCLK 24 MHz // One wait state, if 24 MHz < HCLK 56 MHz // Two wait states, if 56 MHz < HCLK 72 MHz // Prefetch buffer FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); // Flash wait state FLASH_SetLatency(FLASH_Latency_2); // Half cycle access FLASH_HalfCycleAccessCmd(FLASH_HalfCycleAccess_Disable); #endif // EMB_FLASH RCC_HCLKConfig(RCC_SYSCLK_Div1); RCC_PCLK2Config(RCC_HCLK_Div1); RCC_PCLK1Config(RCC_HCLK_Div2); RCC_USBCLKConfig(RCC_USBCLKSource_PLLCLK_1Div5); RCC_ADCCLKConfig(RCC_PCLK2_Div8); // 3. Init PLL RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9); // 72MHz RCC_PLLCmd(ENABLE); // wait until the PLL is ready while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); // 5. Clock system from PLL //RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /*//WAIT FOR PLLCLK TO STABLILZE while(RCC_GetSYSCLKSource() != 0x08) { } */ } void main(void) { GPIO_InitTypeDef GPIO_InitStructure; //SETUP DEBUG #ifdef DEBUG debug(); #endif //CONFIGURE CLOCKS Clk_Init(); // GPIO Init // Enable GPIO clock and release reset RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE | RCC_APB2Periph_GPIOC, ENABLE); RCC_APB2PeriphResetCmd(RCC_APB2Periph_GPIOC, DISABLE); // GPIO_DeInit(GPIOC); // Assign PE6 to LED GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_5 | GPIO_Pin_6; GPIO_Init(GPIOE, &GPIO_InitStructure); // Enaable Swithches on PC0 and PC1 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1; GPIO_Init(GPIOC, &GPIO_InitStructure); //APP MUST NEVER EXIT MAIN FUNCTION. STRANGENESS WILL OCCUR.. while(1) { if(GPIOC->IDR != 0){ GPIOE->BRR = 0x60; } GPIOE->BSRR = 0x60; } } void gpio_flash() { int i; for(i=0;i<300000;i++){ GPIOE->BSRR = 0x60; } for(i=0;i<30000;i++){ GPIOE->BRR = 0x60; } //end gpio_flash } #ifdef DEBUG /******************************************************************************* * Function Name : assert_failed * Description : Reports the name of the source file and the source line number * where the assert_param error has occurred. * Input : - file: pointer to the source file name * - line: assert_param error line source number * Output : None * Return : None *******************************************************************************/ void assert_failed(u8* file, u32 line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* Infinite loop */ while (1) { } } #endif