Shutdown mode for RTC
Hello, I'm using the demoboard B-U585I-IOT02A with a STM32U5 microcontroller. Today, I'm using a RTC with an external battery placed before VBAT. But in order to reduce current consumption, I'm currently working on using shutdown mode in order to just update RTC without using CPU.
My question is the following : If I lose power for Vdd, so only remains Vbat for the RTC (based on the external battery), does the microcontroller go into shutdown mode automatically? Or do I have to do it manually by detecting a power failure just before losing power for the CPU ?
Thanks in advance,