Skip to main content
DavidAlfa
Senior II
September 18, 2021
Question

Shouldn't DMA_HandleTypeDef State be volatile?

  • September 18, 2021
  • 3 replies
  • 867 views

Current structure is:

typedef struct __DMA_HandleTypeDef
{
 ...
HAL_DMA_StateTypeDef State; /*!< DMA transfer state */ 
...
} DMA_HandleTypeDef;

Interrupts can change the State value, but it's not volatile, so the compiler is unaware.

Polling the handler state until it changes to HAL_DMA_STATE_READY will fail when optimizations are enabled.

This works perfectly:

typedef struct __DMA_HandleTypeDef
{
 ...
__IO HAL_DMA_StateTypeDef State; /*!< DMA transfer state */ 
...
} DMA_HandleTypeDef;

This topic has been closed for replies.

3 replies

TDK
September 18, 2021
"If you feel a post has answered your question, please click ""Accept as Solution""."
DavidAlfa
DavidAlfaAuthor
Senior II
September 18, 2021

32F103C8, using FW F1 v1.8.4​ library.

Definitely not in the F1​ library, issued a pull request:

https://github.com/STMicroelectronics/STM32CubeF1/pull/36/commits/4ba3ef94f1d79bd33541f177fd548d4a605dc67a

Piranha
Principal III
September 20, 2021

For this purpose the user is supposed to call the HAL_DMA_GetState() function, which will not have the optimization problem.

Also the Lock member of the structure must be volatile for the compiler to not mess up the access order for these variables.

And they are changing the variables ErrorCode and State after the __HAL_UNLOCK(), which creates a race condition:

https://github.com/STMicroelectronics/STM32CubeH7/blob/ccb11556044540590ca6e45056e6b65cdca2deb2/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma.c#L839

Not counting the ones in HAL_DMA_Init(), which are most likely "by design", they to this after the lines: 656, 752, 839, 877, 949, 1177, 1328, 1373, 1405, 1513, 1541.