Question
Should LSERDY assert with LSEBYP?
Hello,
should LSERDY assert with LSEBYP?
I have a SIT1533 (32.768 khz Mems ocsillator) connected to PC14/OSC32IN on a L412. I first reset the backup domain, than I enable LSEBYP and with next command I enable LSEON. On a cold start, where the SIT1533 may need 500 ms, LSERDY never asserts, also OSCIN is toggling when I check with a scope.
Otherwise why does the sequence
- reset BCDR
- wait that LSERDY is de-asserted
- set LSEBYP
- wait untill LSEBY is asserted
- set LSEON
- wait until LSEON is asserted
- apply clk to OSC32 in
not set LSERDY?