Skip to main content
MMarn.1
Associate
Feb 16, 2023 8:21 AM UTC
Solved

Should I solder and unsolder on the X-NUCLEO-CCA01M1 and X-NUCLEO-CCA02M2 for the Acoustic Echo Cancelling function package ?

I am trying to set-up the demo-kit for Acoustic Echo Cancelling and I am a bit confused about steps 1 and 2 of Getting started with the STM32Cube function pack for acoustic echo cancellation - User manual in part 2.3.1.

On my boards bridges that should be soldered are not but also bridges that should not be soldered are. What does "Configure" means, should I solder every bridge indicated ? And unsolder also the ones that should not be ? Why are resistors highlighted in orange ?

    This topic has been closed for replies.
    MMarn.1
    MMarn.1Best answer
    Associate
    May 11, 2023 2:27 PM UTC

    Hi,

    The support helped me on solving the issues.

    There were 3:

    1- A short circuit caused by J18-19.

    2 - There is a bug in the release v1.2.0 leading to a loud buzzing sound in the loudspeaker.

    It is solved with using version v1.1.0.

    3 - I had an issue when trying to record as both recorded channels were the same.

    This was due to PC audio settings/drivers. To avoid this go to: Sound Control Panel > Recording > STM32MIC + LOUDSPEAKERS > Properties > Advanced > Uncheck "Enable Audio Enhancement."

    3 replies

    Douglas MILLER
    ST Employee
    Feb 22, 2023 5:40 AM UTC

    This forum thread was marked by the moderator as needing a little more investigation, so a Support case was created in your name and will be handled off-line. Should anyone have any similar questions, please feel free to open a Support case directly at your myST portal - https://community.st.com/s/onlinesupport 

    MMarn.1
    MMarn.1AuthorBest answer
    Associate
    May 11, 2023 2:27 PM UTC

    Hi,

    The support helped me on solving the issues.

    There were 3:

    1- A short circuit caused by J18-19.

    2 - There is a bug in the release v1.2.0 leading to a loud buzzing sound in the loudspeaker.

    It is solved with using version v1.1.0.

    3 - I had an issue when trying to record as both recorded channels were the same.

    This was due to PC audio settings/drivers. To avoid this go to: Sound Control Panel > Recording > STM32MIC + LOUDSPEAKERS > Properties > Advanced > Uncheck "Enable Audio Enhancement."

    Associate III
    Aug 14, 2023 4:55 PM UTC

    Hello,

    I'm having the same confusion regarding the configuration of the kits and the nucleo board for Multi-Mic Input (BF, SL, AEC). Its confusing because the diagram has items unsoldered, some soldered and they don't match what's actually on the board. I doubt items should be de-populated... But am still unsure about what exactly should be populated in this case, as it varies significantly.

    I'm following the documentation found here: https://www.st.com/resource/en/data_brief/fp-aud-smartmic1.pdf

    X-NUCLEO-CCA01M1

    PadBoard StatusDocumentation StatusWhat to do?
    J1O  
        
    J17O  
    J3OX 
    J14X  
    J21OX 
    J22O  
        
    J20O  
    J25OX 
    J23O  
        
    J18OX 
    J10XX 
        
    J9XX 
    J12O  
    J6X  
    J15O  
    J2OX 
        
    J11O  
    J13X  
    J8X  
    J5X  
    J24O  
    J4X  
    J16OX 

     

    X-NUCLEO-CCA02M2


    "Solder the external headers to M1_EXT_B and M4_EXT_B". Umm, what external headers, and in what fashion? This is the most undescriptive instruction, because there were no "headers" included with my kit. It was only the board in the plastic package. Are there supposed to be, and otherwise what is the procedure to the use 4 mics in the slots that have headers already?

    PadBoard StatusDocumentation StatusWhat to do?
    SB18O  
    SB19O  
    SB9X  
        
    R1XX 
    R2XX 
    R3O  
    R4XX 
        
    SB8OX 
    SB2XX 
    SB1XX 
        
    SB24O  
    SB10OX 
    SB17O  
    SB11XX 
    SB16O  
    SB15XX 
    SB13XX 
    SB7XX 
    SB26O  
        
    SB21O  
    SB25O  
    SB20O  
        
    SB14O  
    SB12O  
        
    SB22O  
    SB23O  

    I'm also experiencing an issue where after flashing the board with the following: FP-AUD-SMARTMIC1 - STM32Cube function pack for MEMS microphone acquisition, advanced audio processing and audio output - STMicroelectronics it doesn't appear as a "Sound Output" device in windows, only sound input. But I suspect this may be to the board pinout misconfiguration. One problem at a time.

    Can anyone from ST populate the above table on what to do?

    @MMarn.1 I tried to open a ticket for clarification but received an error - "Looks like you don’t have access to create a case. Ask your community manager for access"