Skip to main content
Associate
Jul 4, 2026 2:40 AM UTC
Question

Shortcut of DAC output.

what maximum current the DAC_output / ADC_input pin can hold if shorted to the ground. with internal buffer Off/On? STM32H753zi.

4 replies

Ozone
Principal
Jul 6, 2026 7:11 AM UTC

The datasheet of you specific H7 device ?!?

AlexmanAuthor
Associate
Jul 7, 2026 9:42 AM UTC

datasheet provides the maximum current rating for I/O pins, but not for DAC. while dac pin is also can be I/O, it is only when dac switched off from pin. For a DAC itself, the most i can found is that DAC will reduce voltage for a half with 5kOm load. 
But, no statements about maximum current rate. And no data about possible current at shortcut.

ST Technical Moderator
Jul 6, 2026 7:31 AM UTC

Hi ​@Alexman 

Can you provide full ordering code to check silicon revision or DBGMCU revision ID?

 

The allowable current is limited by the absolute maximum ratings and by the pin’s output drive capability. So it must be checked against the DAC output characteristics and absolute maximum ratings provided in datasheet. You should provide an external current limiting path if the pin is forced to ground.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
AlexmanAuthor
Associate
Jul 7, 2026 9:49 AM UTC

datasheet provides the maximum current rating for I/O pins, but not for DAC. while dac pin is also can be I/O, it is only when dac switched off from pin. For a DAC itself, the most i can found is that DAC will reduce voltage for a half with 5kOm load. 
But, no statements about maximum current rate. And no data about possible current at shortcut.

i am not sure what number you mean. have some :
Customer Part Number
Manufacturer Part Number
Description:
 NUCLEO-H753ZI
STMicro Development Boards & Kits - ARM
JP HS:847150000 ECCN:5A992.C COO:CN
 

Purchase Order Number: ST205468