Skip to main content
contactst
Associate
June 16, 2016
Question

setup for SPI on STM32Cube MX

  • June 16, 2016
  • 2 replies
  • 2192 views
Posted on June 16, 2016 at 18:42

Hello! I don't know setup for SPI NSS software on STM32Cube mx. Anyone help me?

I use stm32f4 discovery and stm32cube mx 4.15.1, SPI1 is master and SPI2 is slave... tks for help!!!

    This topic has been closed for replies.

    2 replies

    slimen
    Visitor II
    June 16, 2016
    Posted on June 16, 2016 at 23:34

    Hello,

    For SPI NSS configuration under STM32CubeMX, you can refer to the

    http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM00104712.pdf/files/DM00104712.pdf/jcr:content/translations/en.DM00104712.pdf

    , it may be helpful.

    You can also refer to the manual

    http://www.st.com/content/ccc/resource/technical/document/reference_manual/4d/ed/bc/89/b5/70/40/dc/DM00135183.pdf/files/DM00135183.pdf/_jcr_content/translations/en.DM00135183.pdf

    , exactly in (26.3 SPI functional description) section to have more idea about configuration hardware SPI NSS.

    Regards

    contactst
    contactstAuthor
    Associate
    June 19, 2016
    Posted on June 19, 2016 at 08:58

    Thank you!!!. can youmodify my code? I want to transmitarr_send_data[10] from SPI2 to SPI3. This my code:

    /**
    ******************************************************************************
    * File Name : main.c
    * Description : Main program body
    ******************************************************************************
    *
    * COPYRIGHT(c) 2016 STMicroelectronics
    *
    * Redistribution and use in source and binary forms, with or without modification,
    * are permitted provided that the following conditions are met:
    * 1. Redistributions of source code must retain the above copyright notice,
    * this list of conditions and the following disclaimer.
    * 2. Redistributions in binary form must reproduce the above copyright notice,
    * this list of conditions and the following disclaimer in the documentation
    * and/or other materials provided with the distribution.
    * 3. Neither the name of STMicroelectronics nor the names of its contributors
    * may be used to endorse or promote products derived from this software
    * without specific prior written permission.
    *
    * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS ''AS IS''
    * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
    * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
    * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
    * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
    * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
    * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
    * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
    * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    ******************************************************************************
    */
    /* Includes ------------------------------------------------------------------*/
    #include ''stm32f4xx_hal.h''
    /* USER CODE BEGIN Includes */
    #define spi_enable HAL_GPIO_WritePin(GPIOB,GPIO_PIN_12,GPIO_PIN_RESET)
    #define spi_disable HAL_GPIO_WritePin(GPIOB,GPIO_PIN_12,GPIO_PIN_SET)
    /* USER CODE END Includes */
    /* Private variables ---------------------------------------------------------*/
    SPI_HandleTypeDef hspi2;
    SPI_HandleTypeDef hspi3;
    /* USER CODE BEGIN PV */
    /* Private variables ---------------------------------------------------------*/
    __IO uint8_t arr_send_data[10] = {15,1,2,3,4,5,6,7,8,9}, arr_receive_data[10];
    //uint8_t send_data,receive_data;
    void SystemClock_Config(void);
    void Error_Handler(void);
    static void MX_GPIO_Init(void);
    static void MX_SPI2_Init(void);
    static void MX_SPI3_Init(void);
    int main(void)
    {
    HAL_Init();
    SystemClock_Config();
    MX_GPIO_Init();
    MX_SPI2_Init();
    MX_SPI3_Init();
    HAL_SPI_Receive_IT(&hspi3,(uint8_t*)arr_receive_data,1);
    while (1)
    {
    spi_enable;
    HAL_SPI_Transmit(&hspi2,(uint8_t*)arr_send_data,2,1000);
    spi_disable;
    }
    }
    void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
    {
    if(hspi->Instance==hspi3.Instance)
    HAL_SPI_Receive_IT(&hspi3,(uint8_t*)arr_receive_data,1);
    }
    /** System Clock Configuration
    */
    void SystemClock_Config(void)
    {
    RCC_OscInitTypeDef RCC_OscInitStruct;
    RCC_ClkInitTypeDef RCC_ClkInitStruct;
    __HAL_RCC_PWR_CLK_ENABLE();
    __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
    RCC_OscInitStruct.HSIState = RCC_HSI_ON;
    RCC_OscInitStruct.HSICalibrationValue = 16;
    RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
    RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
    RCC_OscInitStruct.PLL.PLLM = 8;
    RCC_OscInitStruct.PLL.PLLN = 168;
    RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
    RCC_OscInitStruct.PLL.PLLQ = 4;
    if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
    {
    Error_Handler();
    }
    RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
    |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
    RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
    {
    Error_Handler();
    }
    HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
    HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
    /* SysTick_IRQn interrupt configuration */
    HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
    }
    /* SPI2 init function */
    static void MX_SPI2_Init(void)
    {
    hspi2.Instance = SPI2;
    hspi2.Init.Mode = SPI_MODE_MASTER;
    hspi2.Init.Direction = SPI_DIRECTION_2LINES;
    hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
    hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
    hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
    hspi2.Init.NSS = SPI_NSS_SOFT;
    hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
    hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
    hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
    hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
    hspi2.Init.CRCPolynomial = 10;
    if (HAL_SPI_Init(&hspi2) != HAL_OK)
    {
    Error_Handler();
    }
    }
    /* SPI3 init function */
    static void MX_SPI3_Init(void)
    {
    hspi3.Instance = SPI3;
    hspi3.Init.Mode = SPI_MODE_SLAVE;
    hspi3.Init.Direction = SPI_DIRECTION_2LINES;
    hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
    hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
    hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
    hspi3.Init.NSS = SPI_NSS_HARD_INPUT;
    hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
    hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
    hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
    hspi3.Init.CRCPolynomial = 10;
    if (HAL_SPI_Init(&hspi3) != HAL_OK)
    {
    Error_Handler();
    }
    }
    /** Configure pins as 
    * Analog 
    * Input 
    * Output
    * EVENT_OUT
    * EXTI
    */
    static void MX_GPIO_Init(void)
    {
    GPIO_InitTypeDef GPIO_InitStruct;
    /* GPIO Ports Clock Enable */
    __HAL_RCC_GPIOH_CLK_ENABLE();
    __HAL_RCC_GPIOB_CLK_ENABLE();
    __HAL_RCC_GPIOA_CLK_ENABLE();
    __HAL_RCC_GPIOC_CLK_ENABLE();
    /*Configure GPIO pin Output Level */
    HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12, GPIO_PIN_SET);
    /*Configure GPIO pin : PB12 */
    GPIO_InitStruct.Pin = GPIO_PIN_12;
    GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
    }
    /* USER CODE BEGIN 4 */
    /* USER CODE END 4 */
    /**
    * @brief This function is executed in case of error occurrence.
    * @param None
    * @retval None
    */
    void Error_Handler(void)
    {
    /* USER CODE BEGIN Error_Handler */
    /* User can add his own implementation to report the HAL error return state */
    while(1) 
    {
    }
    /* USER CODE END Error_Handler */ 
    }
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* USER CODE BEGIN 6 */
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* USER CODE END 6 */
    }
    #endif
    /**
    * @}
    */ 
    /**
    * @}
    */ 
    /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/