Skip to main content
santosh
Associate II
Jun 3, 2014 3:04 PM UTC
Question

Setting Timer to 1ms

Posted on June 03, 2014 at 17:04

Hi All,

I am using STM32 F0 Discovery board with Raisonance IDE, I am with LED blink using TIM. I want to blink for every 1s but I dont know how to set the timer, Please tell me how the calculation is done for 1s and 1ms. And what should be the value of Prescalar value,TIM_Period n TIM_Prescaler. Right now I have put random values. Please guide me.

PrescalerValue = (uint16_t) (SystemCoreClock  /2400000 );

 /* Time base configuration */

  TIM_TimeBaseStructure.TIM_Period = 1000;

 TIM_TimeBaseStructure.TIM_Prescaler = 0;

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Down;
    This topic has been closed for replies.

    8 replies

    Tesla DeLorean
    Guru
    Jun 3, 2014 3:39 PM UTC
    Posted on June 03, 2014 at 17:39

    It's simple math using factors, the Prescaler and Period are feed with maximal values, where N ticks are represented as 0 to N-1. The Prescaler is 16-bit, the Period may be 16-bit or 32-bit depending on the timer, not sure on F0 options

    With a 24 MHz clock, 1 ms = 24000 ticks,

    TIM Update = TIM Clock / (X * Y)

    Prescaler = X - 1

    Period = Y - 1

    For 1 ms,

    X = 1, Y = 24000 or

    X = 24, Y = 1000

    For 1 s

    X = 24000, Y = 1000 or

    X = 2400, Y = 10000 or

    X = 800, Y = 30000 or

    X = 400, Y = 60000

    I'd use the UP count mode, one could also drive an LED directly from a TIM channel
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    santosh
    santoshAuthor
    Associate II
    Jun 4, 2014 5:29 AM UTC
    Posted on June 04, 2014 at 07:29

    Hello Clive,

    I set the values as per ur suggestion for 1s but the LED does not blink exactly at 1s, so I have attached the file of my project. Mine is 48MHz so I have adjusted as as per that clock. Appreciate your work. Thanks

    ________________

    Attachments :

    main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0za&d=%2Fa%2F0X0000000bgf%2FnPPkmk_nooBoH4t7splw9qhgt9XwgpM2MUGH5QCbztI&asPdf=false
    Tesla DeLorean
    Guru
    Jun 4, 2014 11:11 AM UTC
    Posted on June 04, 2014 at 13:11

    I don't see any interrupt handling code!

    You want to use the UPDATE interrupt, not CC1
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    santosh
    santoshAuthor
    Associate II
    Jun 4, 2014 11:41 AM UTC
    Posted on June 04, 2014 at 13:41

    Below is my IRQ handler. It is in ''stm32f0xx_it.c''. I replaced CC1 with Update. I can blink the Led for every 1s. But only when 

    Prescaler= 2000

    Period= 24000

    And Blinking time differs for other values which u had mentioned for 1s. Why is it so???

    void TIM14_IRQHandler(void)

    {

        if (TIM_GetITStatus(TIM14, TIM_IT_Update) != RESET)

        {

            TIM_ClearITPendingBit(TIM14, TIM_IT_Update);

            TimingDelay_Decrement();

    }

    }

    Tesla DeLorean
    Guru
    Jun 4, 2014 1:31 PM UTC
    Posted on June 04, 2014 at 15:31

    And Blinking time differs for other values which u had mentioned for 1s. Why is it so???

    Probably because I made the assumption you were using a 24 MHz clocks, and you aren't?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    Jun 4, 2014 1:53 PM UTC
    Posted on June 04, 2014 at 15:53

    This is how I might present an example, a somewhat blind implementation but should be functional

    /* TIM14 1 Hz Toggle STM32F0 sourcer32@gmail.com */
    #include ''stm32f0xx.h''
    /***************************************************************************/
    void RCC_Configuration(void)
    {
    /* GPIOC Periph clock enable */
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
    /* TIM14 clock enable */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM14, ENABLE);
    }
    /***************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    GPIO_SetBits(GPIOC, GPIO_Pin_8);
    GPIO_ResetBits(GPIOC, GPIO_Pin_9);
    }
    /***************************************************************************/
    void NVIC_Configuration(void)
    {
    NVIC_InitTypeDef NVIC_InitStructure;
    /* Enable the TIM14 global Interrupt */
    NVIC_InitStructure.NVIC_IRQChannel = TIM14_IRQn;
    NVIC_InitStructure.NVIC_IRQChannelPriority = 0;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
    }
    /***************************************************************************/
    void TIM_Configuration(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t) (SystemCoreClock / 1000) - 1; // To KHz
    TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // To Hz
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
    TIM_TimeBaseInit(TIM14, &TIM_TimeBaseStructure);
    /* TIM Interrupts enable */
    TIM_ITConfig(TIM14, TIM_IT_Update, ENABLE);
    /* TIM14 enable counter */
    TIM_Cmd(TIM14, ENABLE);
    }
    /***************************************************************************/
    void TIM14_IRQHandler(void)
    {
    if (TIM_GetITStatus(TIM14, TIM_IT_Update) != RESET)
    {
    TIM_ClearITPendingBit(TIM14, TIM_IT_Update);
    /* LED toggling */
    GPIOC->ODR ^= GPIO_Pin_8 | GPIO_Pin_9;
    }
    }
    /***************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    NVIC_Configuration();
    TIM_Configuration();
    /* Infinite loop */
    while (1);
    }
    /***************************************************************************/
    #ifdef USE_FULL_ASSERT
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {}
    }
    #endif
    /***************************************************************************/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    santosh
    santoshAuthor
    Associate II
    Jun 5, 2014 4:11 AM UTC
    Posted on June 05, 2014 at 06:11

    Thank you so much Clive, it worked. Now what should I do for setting 1ms in this

     TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t) (SystemCoreClock  / 1000) - 1; 

      TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // To Hz

    I didn't understand the calculation behind this?? Please

    Tesla DeLorean
    Guru
    Jun 5, 2014 4:28 PM UTC
    Posted on June 05, 2014 at 18:28

    Thank you so much Clive, it worked. Now what should I do for setting 1ms in this

     

    TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t) (SystemCoreClock / 1000) - 1;

     

    TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // To Hz I didn't understand the calculation behind this?? Please

    I explained the math earlier, you are dividing a source clock with two factors.   1 ms   TIM_TimeBaseStructure.TIM_Prescaler = 0; // No division  TIM_TimeBaseStructure.TIM_Period = (uint16_t) (SystemCoreClock / 1000) - 1; // Clocks for 1/1000th of a second (millisecond)    Understand that 1 second is 48000000 ticks of a 48 MHz clock, 1 millisecond would be 1/1000th of that, ie 48000   The values programmed into the hardware for comparison are N-1 

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..