Question
Setting the I2C timing register values for STM32L073RZ
Hi all,
I am trying to interface a STM32L073RZ to a Si2151 tuner IC using I2C. I keep getting HAL_ERROR everytime i use the HAL_I2C_Master_Transmit function. I used STM32cubeMx to set the I2C parameter settings (freq to 400K) but the generated code has hi2c1.Init.Timing = 0x00000000; which i am not sure is correct. Do i need to edit this timing manually ? I found an I2C timing register config tool but that was for STM32F series and not the L series.
Any help is greatly appreciated..
Thanks,
H