Skip to main content
SLevi.1
Associate III
January 9, 2024
Solved

Setting RDP option byte in STM32L452

I have a problem programmatically setting RDP to level 1.

My code is:

OBInit.RDPLevel = OB_RDP_LEVEL_1;
OBInit.OptionType = OPTIONBYTE_RDP;
ret = HAL_FLASH_Unlock();
ret = HAL_FLASH_OB_Unlock();
/* Clear SR register */
CLEAR_BIT(FLASH->SR, FLASH_SR_BSY);
ret = HAL_FLASHEx_OBProgram(&OBInit);
ret = HAL_FLASH_OB_Lock();
ret = HAL_FLASH_Lock();
HAL_Delay(2000);
ret = HAL_FLASH_OB_Launch();
// shouldn't get to this point, as processor will reset

I had to put in the clear pf FLASH->SR, otherwise the "FLASH_WaitForLastOperation" would fail inside "FLASH_OB_RDPConfig". I've no idea why the flash should be busy at this stage.

Whether or not I run this under the debugger, the RDP byte never changes. The last HAL_Delay is to give the flash chance to be written properly before the launch resets the processor.

This topic has been closed for replies.
TDK
TDKBest answer
January 9, 2024

The BSY bit is read-only. Wait for BSY to be low, you can't set it to a value.

You must call HAL_FLASH_OB_Launch before locking option bytes. Locking them prevents access.

Several examples out there for this. Here is one:

https://github.com/STMicroelectronics/STM32CubeL4/blob/93f2cde30d17996651d7b31f7091ab3dfe2f99bb/Projects/NUCLEO-L4R5ZI/Examples/FLASH/FLASH_WriteProtection/Src/main.c#L299

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
January 9, 2024

The BSY bit is read-only. Wait for BSY to be low, you can't set it to a value.

You must call HAL_FLASH_OB_Launch before locking option bytes. Locking them prevents access.

Several examples out there for this. Here is one:

https://github.com/STMicroelectronics/STM32CubeL4/blob/93f2cde30d17996651d7b31f7091ab3dfe2f99bb/Projects/NUCLEO-L4R5ZI/Examples/FLASH/FLASH_WriteProtection/Src/main.c#L299

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pierre_Paris
ST Employee
January 9, 2024

Hello @SLevi.1, and @TDK,

I add this article named How to program STM32 Option Bytes with the HAL API.

Enjoy your reading ! :)

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.