Skip to main content
Associate III
Dec 16, 2024 11:29 PM UTC
Solved

Setting GPIO interrupts for two identical pins

We are developing a software application that uses GPIO interrupts.
We want to set interrupts on the same pins (PE8, PG8), but only one of them can be set to external interrupt mode in the ioc.
Is it not possible to set external interrupt mode for two different ports on the same pin?

This topic has been closed for replies.
Karl Yamashita
Karl YamashitaBest answer
Principal
Dec 17, 2024 12:42 AM UTC

Architecturally it's not possible even if you enabled them in FW. Only one will physically interrupt.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source

2 replies

Karl Yamashita
Karl YamashitaBest answer
Principal
Dec 17, 2024 12:42 AM UTC

Architecturally it's not possible even if you enabled them in FW. Only one will physically interrupt.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate III
Dec 23, 2024 9:09 AM UTC

Thank you for your reply.
We understand that this is a physical constraint, so I will close this.