Associate III
Apr 3, 2026 7:20 AM UTC
Question
Set up PWR_SMPS_1V8_SUPLLY_LDO STM32H755ZIT6
- 5 replies
- 527 views
Dear al!
i need your help, i design PCB use STM32H755ZIT6, i set up mode PWR_SMPS_1V8_SUPLLY_LDO via STM32CubeMX 6.12.1. I expect core M7's clock is 400Mhz, M4's clock is 200Mhz. I measure voltage after L2 is 1.8V, at each Vcap pin is 1.0V, The MCU warmed up to about 35 degrees Celsius and chip didn't run. can you share me my mistake, this is the first time which i handle with SMPS block