Skip to main content
ecatala
Associate II
November 6, 2013
Question

Set FLASH level protection from Level 1 to Level 0

  • November 6, 2013
  • 2 replies
  • 833 views
Posted on November 06, 2013 at 12:23

I am programming the STM32F051x6 micro with the IAR Embedded Workbench IDE and the ST-LINK.

I erased the Flash option bytes and now I can not load my application code into the micro with the ST-LINK because the Flash is in Level1 (read protection).

The manual said that in order to go back to Level0 (no protection)  I have to change the RDP value to 0xAA and that I have to do that executing in user mode.

How can I execute in user mode? Or how can I set the RDP value to 0xAA?

Thanks in advance
    This topic has been closed for replies.

    2 replies

    Amel NASRI
    ST Technical Moderator
    November 6, 2013
    Posted on November 06, 2013 at 12:38

    You can use the 

    http://www.st.com/web/en/catalog/tools/PF258168

    to update protection level and option bytes.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    ecatala
    ecatalaAuthor
    Associate II
    November 6, 2013
    Posted on November 06, 2013 at 13:20

    Thanks. It worked!

    What I wanted to do initially was to program the 2 user bytes (located in the option byes Flash) to store some data. Do you know how Can I progrma these 2 bytes mantaining the level protection to 0? Or is it better I use a standard flash sector to program 2 bytes to store data?