Skip to main content
Visitor II
May 22, 2024
Question

SerialPort with registers

Hello, I am trying to do one simple task with my STM32 board using just registers and interruptions in USART2.

Basically I have to wait until I receive data via serialPort, then activate interruption that should increment the value of my data by 1. After this it should send via serialPort the new data incremented by 1 and wait for the next time it receives data.

Here is the code I implemented:

void serialPrint(USART_TypeDef *dir, uint8_t* data, uint32_t tam) {
 for (uint32_t i = 0; i < tam; i++) {
 dir->DR = data[i];
 while (!(dir->SR & USART_SR_TC)); 
 }
}

void serialScan(USART_TypeDef *dir, uint8_t* data, uint32_t tam) {
 for (uint32_t i = 0; i < tam; i++) {
 while (!(dir->SR & USART_SR_RXNE)); 
 data[i] = dir->DR;
 }
}

void serialScanIT(USART_TypeDef *dir, uint8_t* buf, uint32_t size) {

 uint32_t *NVIC_ISER1 = (uint32_t*)0xE000E104U;
 *NVIC_ISER1 = 0x40;
}

void USART2_IRQHandler(void) {
 if (USART2->SR & USART_SR_RXNE) { 
 dato[pos] = USART2->DR; 
 pos++;
 if (pos >= size) {
 callback(data);
 deactivateIT(); 
 }
 }
}

 

This topic has been closed for replies.

1 reply

Pavel A.
May 24, 2024

Here you can find help with reviewing your code and development of your STM32 project:

https://www.fiverr.com/categories/programming-tech/electronics-engineering/embedded-systems-iot?ref=platform%3Astm32