Skip to main content
anjana087
Associate II
Nov 2, 2016 7:09 AM UTC
Question

serial communication using interrupts

Posted on November 02, 2016 at 08:09

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    1 reply

    Walid FTITI_O
    Visitor II
    Nov 3, 2016 4:41 PM UTC
    Posted on November 03, 2016 at 17:41

    Hi m.anjana,

    First you should check if the NVIC is configured forUSART1_IRQn insidestm32f1xx_hal_msp.c. If it is not, you should enable the NVIC interrupt in the USART configuration window of CubeMX. Second , you should initialize the data buffer as global and not local , the you pass it as pointer inside the USART interrupt transfer start function . The receive should start after checking the transfer has really complete by managing a ready flag. See example below:

    /*- Start the transmission process */

    if(HAL_UART_Transmit_IT(&UartHandle, (uint8_t*)DataTX, DataTX_SIZE)!= HAL_OK) { Error_Handler(); } /*##-3- Wait for the end of the transfer ###################################*/ while (UartReady != SET) { } /* Reset transmission flag */ UartReady = RESET; /*##-4- Put UART peripheral in reception process ###########################*/ if(HAL_UART_Receive_IT(&UartHandle, (uint8_t *)DataRX, DataRX_SIZE) != HAL_OK) { Error_Handler(); } Third, you manage the UartReady flag inside the Tx call back as follow :

    void HAL_UART_TxCpltCallback(UART_HandleTypeDef *UartHandle)
    {
    /* Set transmission flag: transfer complete */
    UartReady = SET;
    }

    -Hannibal-