Skip to main content
Associate
Aug 20, 2024 6:08 PM UTC
Solved

Serial Communication between STM32 High Performance MCU and Time Delay DS1023

Hello, 

I need to implement a serial communication between MCU such as STM32F4xx or STM32F2xx and a Time Delay DS1023 but its datasheet doesn´t mention any standard communication protocol such as SPI.

Could i use three GPIOs as Serial Input, Serial Output and Latch Enable besides a MCO (Master Clock Output) pin (used as CLK) to implement it?

In case it is a possible solution or, in case there is a better way, knowing that will help me to decide which items to buy and how to do it.

Thanks in advance!

Alejandro Pinto

 

.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 20, 2024 6:39 PM UTC

Welcome @AlejandroPinto, to the community!

The first thing that springs to mind with such tasks is bit banging using some GPIO pins, which is perfectly feasible. After a cursory glance at the data sheet, however, I was able to see that you can also use an SPI port for serial communication - the timing of the SPI port would just have to be configured correctly. Details can be found in the reference manual of the respective STM32.

Please note that this is an old 5V device that requires a separate 5V supply. Fortunately, its CMOS inputs are almost TTL compatible, so you can control the device directly from the STM32 without a level shifter.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 20, 2024 6:39 PM UTC

Welcome @AlejandroPinto, to the community!

The first thing that springs to mind with such tasks is bit banging using some GPIO pins, which is perfectly feasible. After a cursory glance at the data sheet, however, I was able to see that you can also use an SPI port for serial communication - the timing of the SPI port would just have to be configured correctly. Details can be found in the reference manual of the respective STM32.

Please note that this is an old 5V device that requires a separate 5V supply. Fortunately, its CMOS inputs are almost TTL compatible, so you can control the device directly from the STM32 without a level shifter.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Aug 28, 2024 4:25 PM UTC

Thank you very much for your response Peter!

Best regards,

Alejandro Pinto