Skip to main content
Gabriel T
Senior
Nov 2, 2020 8:54 AM UTC
Question

Send reset with DFU using Cubeprogrammer Api

Hello,

I am using STM32 CubeProgrammer Api and I succesfully bootload my STM32H743ZI but it stays in bootloader mode after download, is there any way to ask a reset ?

There is a reset function in the dll but it specify that it only works in SWD/JTAG mode :

/**
 * \brief This routine used to apply a target reset.
 * \note Reset operation is only available with JTAG/SWD debug interface.
 * \param rstMode : Indicates the reset type Soft/Hard/Core #debugResetMode. \n
 * \return 0 if the reset operation finished successfully, otherwise an error occurred.
 */
int reset(debugResetMode rstMode) ;

Is it possible to send a reset intruction in DFU while the MCU is in bootloader mode ?

It should be possible because the STM32 Cube Programmer software is able to do a reset after programming.

Regards

    This topic has been closed for replies.