Skip to main content
ganesh23
Visitor II
April 21, 2012
Question

selection of accelrerometer IC for car crash detection

  • April 21, 2012
  • 1 reply
  • 566 views
Posted on April 21, 2012 at 07:42

seection of accelrerometer IC for car crash detection. which parameter need to consider,

please suggest which IC is best.

Which g level is required.

please let me know

thank you
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 21, 2012
    Posted on April 21, 2012 at 14:14

    You need to find someone qualified to answer/develop the solution. Random people on the internet should not be relied upon for life critical design parameters.

    You need to know the initial speed/velocity, and the time/distance required to come to rest.

    You might be able to get some number from local insurance/government labs about the forces in crashes from vehicle crash testing. The results from USA might not be applicable to vehicles in other markets with more lax safety requirements.

    The G forces of hitting a concrete wall at speed are going to be very high, it's going to stop very quickly and the distance travelled will be the deformation of the vehicle. Hitting a pedestrian at similar speeds will have significantly less impact. Many accidents are considered insufficient to deploy an air bag, and depend on the direction of the impact.

    http://www.hwycom.com/safetyCrashTest60.php

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..