Skip to main content
Associate II
Dec 31, 2025 3:23 AM UTC
Solved

Seeking STM32 MCU with Dual USB 2.0 High-Speed (480Mbps)

Hi Sir,

Does any STM32 MCU support two independent USB 2.0 High-Speed (480 Mbps) interfaces simultaneously? I have observed that current H7 parts limit the second core to Full-Speed only. Do any newer series support true dual-HS operation?

Thank you.

TDK
TDKBest answer
Dec 31, 2025 3:45 AM UTC

@TIENHUA wrote:

Does any STM32 MCU support two independent USB 2.0 High-Speed (480 Mbps) interfaces simultaneously?


Nope. Just 1 HS + 1 FS max on a few different families.

Introduction to USB hardware and PCB guidelines using STM32 MCUs - Application note

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Dec 31, 2025 3:45 AM UTC

@TIENHUA wrote:

Does any STM32 MCU support two independent USB 2.0 High-Speed (480 Mbps) interfaces simultaneously?


Nope. Just 1 HS + 1 FS max on a few different families.

Introduction to USB hardware and PCB guidelines using STM32 MCUs - Application note

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Dec 31, 2025 10:30 AM UTC

For all your STM32 device search needs:

STM32 MCU product selector

ST-MCU-FINDER-PC

STM32-FINDER for mobile devices

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.