Skip to main content
Associate
March 19, 2025
Question

SDMMC and USB Mass Storage Class (MSC).

  • March 19, 2025
  • 3 replies
  • 486 views

I am using the STM32H745I-DISCO board, where Core M4 handles SDMMC and FATFS, and Core M7 manages USB Mass Storage Class (MSC). Is there a procedure or any available documentation on linking both cores for seamless data sharing?

This topic has been closed for replies.

3 replies

Pavel A.
March 19, 2025

Sharing which data? Do you mean, sharing the filesystem on SD card between the CM4 and CM4 applications? (like, both CM4 and CM7 can create files on the SDcard?)

 

indhujaAuthor
Associate
March 20, 2025

No. File system should create in m4 , Only file access needs to be implemented in USB.

1. Write all sensor data in flash through m4.

2. Collect stored data through M7 via USB mass storage

Pavel A.
March 20, 2025

Very good, so the CM4 and CM7 just need to send data between them. Use any internal RAM that can be shared between them, and hardware semaphores for synchronization.