Question
SDIO STM32F215 need help
Posted on August 12, 2011 at 15:05
I have no clock on PC12. But when PC12 is OUT mode it is work.
If I run mySDInit() I will see two jump on pc12 ( out mode test ). No clock. Where is the bug?void mySDInit( void ){
uint32_t regSDIO_CLKCR;GPIO_InitTypeDef GPIO_InitStructure;
SDIO_InitTypeDef SDIO_InitStructure;/* GPIOC and GPIOD Periph clock enable */
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOD, ENABLE ); /* Enable the SDIO APB2 Clock */ RCC_APB2PeriphClockCmd( RCC_APB2Periph_SDIO, ENABLE );/* Configure PC.12 pin: CLK pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIOC->BSRRL = GPIO_Pin_12; GPIOC->BSRRH = GPIO_Pin_12; GPIOC->BSRRL = GPIO_Pin_12; GPIOC->BSRRH = GPIO_Pin_12;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_Init(GPIOC, &GPIO_InitStructure); /* Configure PD.02 CMD line */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOD, &GPIO_InitStructure);/* Configure PC.08, PC.09, PC.10, PC.11 pins: D0, D1, D2, D3 pins */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOD, GPIO_PinSource2, GPIO_AF_SDIO);RCC_APB2PeriphResetCmd(RCC_APB2Periph_SDIO, ENABLE);
RCC_APB2PeriphResetCmd(RCC_APB2Periph_SDIO, DISABLE); SDIO_InitStructure.SDIO_ClockDiv = SDIO_INIT_CLK_DIV; SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising; SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Enable; SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable; SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_1b; SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable; SDIO_Init(&SDIO_InitStructure);/*!< Set Power State to ON */
SDIO_SetPowerState(SDIO_PowerState_ON);/*!< Enable SDIO Clock */
SDIO_ClockCmd(ENABLE); regSDIO_CLKCR = SDIO->CLKCR; while( 1 ); }