Skip to main content
zbyszekl
Associate II
December 11, 2012
Question

SDIO in STM32F2XX

  • December 11, 2012
  • 3 replies
  • 1084 views
Posted on December 11, 2012 at 01:56

Can an interface SDIO in STM32F2XX read/write micro SDHC UHS-1 cards?

Are there any examples, experience of this type of  operation?

What was the maximum speed of writing to the card?

#sdio-stm32f2xx-microsdhc-uhs-1
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
December 11, 2012
Posted on December 11, 2012 at 18:09

I have a card on order now the prices have come down to more reasonable levels.

I suspect the hardware will support them, the software may need to be changed to address any command issues, and the 64GB cards are supposed to use FATX which is not supported by versions of FatFs I've looked at.

I would not expect it to be particularly fast, or any faster than a current CLASS 10 SDHC card.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
zbyszekl
zbyszeklAuthor
Associate II
December 11, 2012
Posted on December 12, 2012 at 00:46

Thanks Clive,

If estimated speed is aprox 10MB/s I'll stay with micro SDHC cards.

Tesla DeLorean
Guru
December 14, 2012
Posted on December 14, 2012 at 16:48

64MB UHS Speed Class 1, Class 10

http://www.sandisk.com/products/memory-cards/microsd/ultra-class10-for-android/?capacity=64GB

Quick benchmark on a 120 MHz STM32F2

51200 Bytes, 565424 Cycles                                                      

10,866,182 Bps Read                                                             

51200 Bytes, 745913 Cycles                                                      

 8,236,886 Bps Write                                                             

 

No changes to the software. Seen similar card read at 19 MBps on PC's, supposedly rated at 30 MBps. There are other SanDisk parts quoted in the 90-95 MBps region, but I don't have or plan to get any of those.

Figure the top write speed on hardware that can clock the interface harder, you might get 11 MBps

http://www.androidpolice.com/2012/05/27/quick-look-sandisk-64gb-microsdxc-ultra-high-speed-card-a-fitting-name/

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..