Skip to main content
This topic has been closed for replies.
pedro23
pedro23Best answer
Associate III
Aug 2, 2019 4:54 PM UTC

Ok then problem was the buffer that i was using, its address was 0x10000400 instead of a 0x200xxxxx address

5 replies

pedro23
pedro23Author
Associate III
Aug 2, 2019 8:30 AM UTC

With DMA it hangs on SD_WaitReadOperation(); With polling it is ok. Btw, any speed adventage polling vs dma?

 void NVIC_Configuration_SD(void)
{
 NVIC_InitTypeDef NVIC_InitStructure;
 
 // Configure the NVIC Preemption Priority Bits
 NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);
 	// SDIO Interrupt ENABLE
 NVIC_InitStructure.NVIC_IRQChannel = SDIO_IRQn;
 NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
 NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
 NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
 NVIC_Init(&NVIC_InitStructure);
 // DMA2 STREAMx Interrupt ENABLE
 NVIC_InitStructure.NVIC_IRQChannel = SD_SDIO_DMA_IRQn;
 NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
 NVIC_Init(&NVIC_InitStructure);
}
 
void main(void)
{
 
System_Setup();
 
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
 
SD_Init();
NVIC_Configuration_SD();
int Status;
uint16_t Error;
for(int i=0;i<125;i++)
{
 
 Debugprintf("Sector: %d",i);
 Status = SD_ReadBlock ( (uint8_t *) Scr, i<<9, 512);
 Status = SD_WaitReadOperation();
 while(SD_GetStatus() != SD_TRANSFER_OK);
 Debugprintf(" RD Status: %d",Status);
 Error=0;
 for(int j=0;j<512;j++)
 if(((uint8_t *) Scr)[i]!=(i+1))
 Error++;
 if(Error)
 {
 Debugprintf(" RD Error: %d",Error);
 memset((uint8_t *) Scr,i+1,512);
 do 
 {
 Status=SD_WriteBlock ( (uint8_t *) Scr, i<<9 , 512);
 Status = SD_WaitWriteOperation();
 while(SD_GetStatus() != SD_TRANSFER_OK);
 Debugprintf(" WR Status: %d",Status);
 }while(Status);
 } 
 else 
 Debugprintf(" NO ERROR"); 
}
while(1)
 IWDG_ReloadCounter();

pedro23
pedro23Author
Associate III
Aug 2, 2019 10:29 AM UTC

Adding more information it calls SDIO_IRQHandler but it is not calling SD_SDIO_DMA_IRQHANDLER interrupt

void SDIO_IRQHandler(void)
{
	SD_ProcessIRQ();
}
 
void SD_SDIO_DMA_IRQHANDLER(void)
{
	SD_ProcessDMAIRQ();
}

Tesla DeLorean
Guru
Aug 2, 2019 1:00 PM UTC

What part?

Double check IRQ Handler name and linkage via .MAP file and inspection of vector table.

Inspect peripheral registers for DMA, SDIO and RCC in debugger.

Review DMA unit/channel settings and initialization

Check if SDIO IRQ firing for transfer actually completing

Advantage of DMA is that it isn't affected by interrupt loading, and less affected by bus loading against LTDC traffic.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
pedro23
pedro23Author
Associate III
Aug 2, 2019 4:35 PM UTC

I have been checking and all seems ok

Yes, SDIO IRQ fires with error SD_RX_OVERRUN when reading, than then it hangs on SD_WaitReadOperation here:

while(((SDIO->STA & SDIO_FLAG_RXACT)) && (timeout > 0))
 {
 timeout--;
 }
 

pedro23
pedro23AuthorBest answer
Associate III
Aug 2, 2019 4:54 PM UTC

Ok then problem was the buffer that i was using, its address was 0x10000400 instead of a 0x200xxxxx address