Skip to main content
konoppo
Associate II
September 12, 2012
Question

SDIO Data Timeout timer doesn't start

  • September 12, 2012
  • 1 reply
  • 697 views
Posted on September 12, 2012 at 08:57

Hi!

   I've got another problem with my STM32F205. The Data Timeout timer doesn't start and when there is no answer from SD Card, the system waits in loop for watchdog reset ;). 

Here is a function. The code is working properly but sometimes (after re-init of the card) it hangs up. 

SD_Error SD_SendSDStatus(uint32_t *psdstatus)

{

  SD_Error errorstatus = SD_OK;

  uint32_t count = 0;

  if (SDIO_GetResponse(SDIO_RESP1) & SD_CARD_LOCKED)

  {

    errorstatus = SD_LOCK_UNLOCK_FAILED;

    return(errorstatus);

  }

  /*!< Set block size for card if it is not equal to current block size for card. */

  SDIO_CmdInitStructure.SDIO_Argument = 64;

  SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_SET_BLOCKLEN;

  SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short;

  SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No;

  SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable;

  SDIO_SendCommand(&SDIO_CmdInitStructure);

  errorstatus = CmdResp1Error(SD_CMD_SET_BLOCKLEN);

  if (errorstatus != SD_OK)

  {

    return(errorstatus);

  }

  /*!< CMD55 */

  SDIO_CmdInitStructure.SDIO_Argument = (uint32_t) RCA << 16;

  SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_APP_CMD;

  SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short;

  SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No;

  SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable;

  SDIO_SendCommand(&SDIO_CmdInitStructure);

  errorstatus = CmdResp1Error(SD_CMD_APP_CMD);

  if (errorstatus != SD_OK)

  {

    return(errorstatus);

  }

  SDIO_DataInitStructure.SDIO_DataTimeOut = 0x10000;

  SDIO_DataInitStructure.SDIO_DataLength = 64;

  SDIO_DataInitStructure.SDIO_DataBlockSize = SDIO_DataBlockSize_64b;

  SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToSDIO;

  SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block;

  SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;

  SDIO_DataConfig(&SDIO_DataInitStructure);

  /*!< Send ACMD13 SD_APP_STAUS  with argument as card's RCA.*/

  SDIO_CmdInitStructure.SDIO_Argument = 0;

  SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_SD_APP_STAUS;

  SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short;

  SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No;

  SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable;

  SDIO_SendCommand(&SDIO_CmdInitStructure);

  errorstatus = CmdResp1Error(SD_CMD_SD_APP_STAUS);

  if (errorstatus != SD_OK)

  {

    return(errorstatus);

  }

 

while (!(SDIO->STA &(SDIO_FLAG_RXOVERR | SDIO_FLAG_DCRCFAIL | SDIO_FLAG_DTIMEOUT | SDIO_FLAG_DBCKEND | SDIO_FLAG_STBITERR)))

  {

    if (SDIO_GetFlagStatus(SDIO_FLAG_RXFIFOHF) != RESET)

    {

      for (count = 0; count < 8; count++)

      {

        *(psdstatus + count) = SDIO_ReadData();

      }

      psdstatus += 8;

    }

  }

The

red while

sometimes never ends. Why the DataTimeout do not occur? Why it not even starts? When I stop my program and watch the SDIO->DTIMER value it's still on the start value. I wan't to rewrite the library by own, because it's not ''FreeRTOS ready'', but I must understand how it works and why it's not working as I think. 

Thanks for Your help

Best regards

Konoppo

#sdio #timeout
This topic has been closed for replies.

1 reply

ta_it
Associate
February 17, 2014
Posted on February 17, 2014 at 12:02

Hello,

Did you find solution for this? It happens frequently in my project.