Skip to main content
carl2399
Associate III
July 27, 2012
Question

SD Command Timeout

  • July 27, 2012
  • 4 replies
  • 2186 views
Posted on July 27, 2012 at 02:58

Just curious if any one else has issues with, or has a workaround for an issue I've been experiencing with the SDIO controller on STM32F20x devices.

I'm developing a data logging that writes data to SD card at the rate of about 2K bytes per second. I've got DMA transfer and also multi-block transfers working fine and have verified bulk transfer speeds around 6M bytes per second. 

The problem is that every once in a while (several thousand block writes) I get a command timeout. I've read a fair bit on the web about people having similar issues (typically with SD_CMD_SET_BLOCKLEN). However, if I get rid of ''spurious'' block length setting then the same error just moves to sequentially the next command along (typically SD_CMD_WRITE_SINGLE_BLOCK).

I guess my question is twofold:

1) Is there a known cause? Something that I could maybe detect beforehand.

2) Is there a ''best sequence'' to recover from this state back to normal operations?

    This topic has been closed for replies.

    4 replies

    amin23
    Visitor II
    August 2, 2012
    Posted on August 02, 2012 at 09:19

    Hi,

    Add the following lines after SD_Write function:

    status = SD_WaitWriteOperation();

    while(SD_GetStatus() != SD_TRANSFER_OK);

    if (status == SD_OK)

    {

      //OK;

    }

    else

    {

      //ERROR;

    }

    frankmeyer9
    Associate III
    August 2, 2012
    Posted on August 02, 2012 at 10:16

    The problem is that every once in a while (several thousand block writes) I get a command timeout.

     

    Could it possible that the timeout happens if an actual block erase is involved ?

    Moritz M
    Associate II
    November 21, 2012
    Posted on November 21, 2012 at 18:44

    Hi CJacobs,

    I'm experiencing the same problem (randomly occurring command timeout with SD_CMD_SET_BLOCKLEN) on a STM32F1xx.

    Did you find a solution for your problems?

    Moritz M
    Associate II
    November 22, 2012
    Posted on November 22, 2012 at 17:16

    so i solved my problem. it was, that the card was still busy when tried to send a new command.