Skip to main content
Visitor II
January 18, 2024
Question

SD Card SDIO not working(FR_DISK_ERR)

  • January 18, 2024
  • 2 replies
  • 845 views

I have a custom board and I have to run an SD card on it using SDIO protocol however on f_mount() function it takes a long time to come out with error FR_DISK_ERR but when I call "HAL_SD_GetCardInfo(&hsd, &sdCardSpace)" then I am getting all the data. I have tried with both 1-bit and 4-bit SDIO and DMA but none is working. I need help to figure out if its hardware error or software error or what the error is.

This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
January 29, 2024

Hello @fs_it and welcome to the Community :),

Could you please precise, which STM32 device are you using?

Do you use the STM32CubeMX for code generation?

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
January 29, 2024

Also, try to check the SDcard on another device PC/laptop or others .. It could be an issue on the SDcard you are using!

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.