Skip to main content
Entwicklung Rauch
Visitor II
October 24, 2017
Question

SD-Card problem (X-NUCLEO-IDW04A1)

  • October 24, 2017
  • 0 replies
  • 562 views
Posted on October 24, 2017 at 15:03

Hello!

I'm using the X-NUCLEO-IDW04A1 evaluation board. The problem is that I can't communicate with the SD card. I've tried the following AT commands 'AT+S.FSC=test.txt, 1000', 'AT+S.FSC=0:test.txt, 1000' and 'AT+S.FSC=0:/test.txt, 1000'. Can someone help me please?

#spwf04sa #sd-card #idw04a1
This topic has been closed for replies.