Skip to main content
donev_g
Associate II
November 22, 2013
Question

SD card Lock/Unlock example

  • November 22, 2013
  • 5 replies
  • 4978 views
Posted on November 22, 2013 at 14:27

Hi All,

Does anybody have an example how to lock/unlock SD card using SDIO and CMD42?
    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    November 22, 2013
    Posted on November 22, 2013 at 16:54

    Does anybody have an example how to lock/unlock SD card using SDIO and CMD42?

    No, but I might entertain an offer, or bounty for such.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    SPasz
    Visitor II
    November 9, 2018

    Do you have working code example Clive?

    Tesla DeLorean
    Guru
    November 9, 2018

    Nothing recent, I've done it with ATA devices previously.

    What STM32 platform? What generation of cards or chips?

    I personally prefer end-to-end encryption, it is less open to broken/compromised implementation, and government interference.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    donev_g
    donev_gAuthor
    Associate II
    November 22, 2013
    Posted on November 22, 2013 at 17:34

    Thanks clive!

    donev_g
    donev_gAuthor
    Associate II
    November 27, 2013
    Posted on November 27, 2013 at 17:07

    Here is my code, if somebody can help:

    void SD_SetPDW_Test(void){

    SD_Error x = SD_Init();

         errorstatus = SD_GetCardStatus(&cardstatus);

         SDIO_CmdInitStructure.SDIO_Argument = 10;

         SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_SET_BLOCKLEN;

         SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short;

         SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No;

         SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable;

         SDIO_SendCommand(&SDIO_CmdInitStructure);

       

         errorstatus = CmdResp1Error(SD_CMD_SET_BLOCKLEN);

       SDIO_CmdInitStructure.SDIO_Argument = 0;

       SDIO_CmdInitStructure.SDIO_CmdIndex = SD_CMD_LOCK_UNLOCK;

       SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_Short;

       SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No;

       SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable;

       SDIO_SendCommand(&SDIO_CmdInitStructure);

         SDIO_DataInitStructure.SDIO_DataTimeOut = SD_DATATIMEOUT;

         SDIO_DataInitStructure.SDIO_DataLength = 11;

         SDIO_DataInitStructure.SDIO_DataBlockSize = SDIO_DataBlockSize_16b; //SDIO_DataBlockSize_16b;

         SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToCard;

         SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block;

         SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;

         SDIO_DataConfig(&SDIO_DataInitStructure);

     memset(tmp_buff, 0, 64);

     

     memcpy(&(tmp_buff[3]), passw, sizeof(passw));

     

     uint8_t csCalc[10] = {SD_SET_PWD_SDIO | SD_LOCK_UNLOCK_SDIO, 6, 'A', 'D' , '3', '2', '4', 'Z', 0x65, 0x41 }; //password is AD324Z and the checksum CRC/CCIT(16 bit) is 0x4165

       SDIO_ITConfig(SDIO_IT_DCRCFAIL | SDIO_IT_DTIMEOUT | SDIO_IT_DATAEND | SDIO_IT_RXOVERR | SDIO_IT_STBITERR, ENABLE);

       SD_LowLevel_DMA_TxConfig((uint32_t *)csCalc, 10);

       SDIO_DMACmd(ENABLE);

       errorstatus = CmdResp1Error(SD_CMD_LOCK_UNLOCK); //here the status is SD_OK

       errorstatus = SD_GetCardStatus(&cardstatus); //here the status is SD_OK but probably should be SD_LOCKED

      

      } At the end SD card status returns SD_OK but I think that it should be SD_LOCKED. And the SD card is not locked.