Solved
Screen is terminating
Hi, I'm using an STM32F401RE board for a class(programming using MacOS). Right now, I'm using VSCode and make to edit and compile my code, then using stlink to flash it. All I'm trying to do is print hello world to the tty.usbmodem* screen in the /dev/ directory. To do this, I'm using the screen /dev/tty.usbmodem* but all I'm getting is [screen is terminating] anyone know why?
Here is my code:
while (1) {
HAL_GPIO_TogglePin(GPIOA, LD2_Pin);
strcpy((char*)buf, "hello world!\r\n");
HAL_UART_Transmit(&huart2, buf, strlen((char*)buf), HAL_MAX_DELAY);
HAL_Delay(500);
}