Skip to main content
FFran.2
Associate
August 30, 2022
Question

SAI serial audio interface. I can't read right channel samples.

  • August 30, 2022
  • 2 replies
  • 711 views

NUCLEO-H743ZI2 board 

SAI A1 16bit data, 2 slot as slave.

codec TLV320AIC23BIPW , clock 12MHz, I2S mode 46.8KHz BCLK=3MHz.

I can read the samples of the left channel correctly. I can't read right channel samples.

static void MX_SAI1_Init(void)

{

 /* USER CODE BEGIN SAI1_Init 0 */

 /* USER CODE END SAI1_Init 0 */

 /* USER CODE BEGIN SAI1_Init 1 */

 /* USER CODE END SAI1_Init 1 */

 hsai_BlockA1.Instance = SAI1_Block_A;

 hsai_BlockA1.Init.AudioMode = SAI_MODESLAVE_RX;

 hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS;

 hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;

 hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;

 hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;

 hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE;

 hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING;

 hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED;

 if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_MSBJUSTIFIED, SAI_PROTOCOL_DATASIZE_16BIT, 2) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN SAI1_Init 2 */

 /* USER CODE END SAI1_Init 2 */

}

static void MX_DMA_Init(void)

{

 /* DMA controller clock enable */

 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */

 /* DMA1_Stream0_IRQn interrupt configuration */

 HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);

 HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);

}

codec init

uint16_t AIC23REGS[]={

0b0001111000000000, //reg15

0b0000000000010111, //reg0 

0b0000001000010111, //reg1 

0b0000010111111001, //reg2 

0b0000011111111001, //reg3 

0b0000100000010001, //reg4 

0b0000101000000000, //reg5 

0b0000110000000000, //reg6 

0b0000111001000010, //reg7 data format: I2S format , MSB first, left – 1 aligned

0b0001000000000000, //reg8 AIC23_REG8 46.8KHZ Clock mode select: 0=Normal

0b0001001000000001, //reg9 : digital interface activation

};

I start reading

  StatusCodec=HAL_SAI_Receive_DMA(&hsai_BlockA1, pData, Size);

void DMA1_Stream0_IRQHandler(void)

here i found only one channel audio data.

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
August 30, 2022

> SAI A1 16bit data, 2 slot as slave.

You mean, 8bits left, 8 bits right? Or 16 bit each channel? That's 32 bits altogether.

> if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_MSBJUSTIFIED, SAI_PROTOCOL_DATASIZE_16BIT, 2) != HAL_OK)

Maybe not. Who knows what Cube/HAL exactly does with this.

Read out and check the SAI registers content. Or for ultimate solution, ditch Cube and write those registers yourself. It's only 4 registers or so.

JW

FFran.2
FFran.2Author
Associate
August 30, 2022
Il 30/08/2022 11:37, ST Community ha scritto:
thank you for your reply