Skip to main content
T J
Senior III
December 26, 2017
Question

Safe Testing of LoRa

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    December 26, 2017
    Posted on December 26, 2017 at 18:38

    These modules have an STM8 inside, not sure they are designed to work with LoRaWAN, but rather point-to-(multi)point

    Place the antenna above and away from you. Cable the devices so you don't need to touch them, and drop power to lowest levels.

    The Murata 100mW module can get ~1KM with minimal effort. Get about 3KM LoS at higher data rates (31kbps), seen 11KM LoS at the lowest (183bps). It could probably get further, but my local topology isn't helpful, and I'm not inclined to climb 100ft-600ft towers. Seen people report 27KM range where base was up a mountain. I could readily see someone using this for long distance control/telemetry link for a UAV.

    For range testing here I have a base unit periodically beacon a signal, and a rover unit in the truck that beeps when the valid data is received. The counter play is to have the rover beacon a GPS location, and have the base log these and compute distance or plot coverage map.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..