Skip to main content
caleb
Associate III
Feb 8, 2019 1:15 AM UTC
Question

Running STM32H7 at 1.8V with USB High speed ULPI PHY USB3310

Hello all,

I'm building a system that I'd like to run at 1.8V with an STM32H7 and USB high speed PHY.

I have a few questions, so I'll just jump right in:

1) Will the STM32H7 core run at 400MHz when powered by VDD=1.8V? Some MCUs can't run as fast at lower voltages, so I wanted to make sure it'll run fine at 1.8V.

2) Internal (full-speed) phy: As long as I supply VDD33USB I assume it will work fine. However, is 3.3V required on VDD33USB if I'm using an external ULPI phy at 1.8V? The datasheet is not clear. It says in table 22 of STM32H570 datasheet: VDD33USB: USB USED 3.0-3.6V, USB not used: 0-3.6V. I suspect VDD33USB only powers the on-board full-speed PHY, but I'm not sure.

3) Has anybody tried the USB3310 PHY with STM32H devices at 1.8V? It would be great to know if I can expect this to work :)

Thank you so much,

-Caleb

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Feb 8, 2019 4:45 AM UTC

    >>1) Will the STM32H7 core run at 400MHz when powered by VDD=1.8V? Some MCUs can't run as fast at lower voltages, so I wanted to make sure it'll run fine at 1.8V.

    Doesn't it run internally at 1.2V or lower?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    caleb
    calebAuthor
    Associate III
    Feb 8, 2019 5:42 AM UTC

    That's what I thought, but just wanted to be doubly sure