Question
Running application in "Release mode causes errors"
Hi all,
I'm trying to profile my application which running on STM32F469IH6 micro-controller.
I'm able to run the application in debug mode and able to see the timings of the applications.
But In generally running application in release mode will have more optimizations included compared with the debug mode. But If I run the application in Release mode then i'm encountered with below error.
Below is log at the time of running application in release mode:
STMicroelectronics ST-LINK GDB server. Version 5.6.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0-RC1
-------------------------------------------------------------------
ST-LINK SN : 066DFF535254887767171939
ST-LINK FW : V2J37M26
Board : 32F469IDISCOVERY
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x434
Revision ID : Rev A
Device name : STM32F469xx/F467xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a09660.srec
File : ST-LINK_GDB_server_a09660.srec
Size : 676208 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 9]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:12.201
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...
Thanks in advance.