Skip to main content
AP_040
Senior
June 27, 2019
Question

Run application other than 0x08000000 in STM32L4

  • June 27, 2019
  • 6 replies
  • 1210 views

I want to run the application code other than the default location of flash 0x08000000 in STM32 MCU.

For doing this I have modified the VECT_TAB_OFFSET = 0x200 in system_stm32l4xx.c

SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET;

Also, FLASH (rx)   : ORIGIN = 0x8000200, LENGTH = 512K in .ld file.

By doing this changes it is not working. So, apart from this is there any changes still required? Please help me on this.

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
June 27, 2019

The processor always reads the vector table at zero, the BOOTx pins determine what is mapped/shadowed here at start up.

Usually mapped with FLASH from 0x08000000

You can't change it to 0x08000200, but you will need to transfer control there from code or a table referenced at 0x08000000

You have created your image correctly, but the processor won't get there magically.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AP_040
AP_040Author
Senior
June 27, 2019

@Community member​ Can you tell me how to transfer control to 0x08000200 location from table referenced at 0x08000000?

Tesla DeLorean
Guru
June 27, 2019

Replicate the first two table entries, or jump/branch to the entry point

Reset_Handler  PROC

        EXPORT Reset_Handler

; ...

        LDR   R0, =0x08000200 ; Secondary Vector Table

        LDR   SP, [R0, #0] ; Load SP

        LDR   R0, [R0, #4] ; Load PC

        BX   R0 ; Jump too

        ENDP ; Reset_Handler

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AP_040
AP_040Author
Senior
June 28, 2019

@Community member​  I have added above instruction in the startup file but it is giving me the errors:

..\startup\startup_stm32l462xx.s:76: Error: bad instruction `reset_handler PROC'

..\startup\startup_stm32l462xx.s:77: Error: bad instruction `export Reset_Handler'

..\startup\startup_stm32l462xx.s:82: Error: bad instruction `endp Reset_Handler'

I added this at start in the startup file. Is it right? Let me correct if I mistake something, here I attached the my startup file.

Tesla DeLorean
Guru
June 28, 2019

I'm using Keil syntax, you'll need to adapt to GNU/GAS if that is what you're using.

Just take the body of the code

    LDR   R0, =0x08000200 /* Secondary Vector Table */

        LDR   SP, [R0, #0] /* Load SP */

        LDR   R0, [R0, #4] /* Load PC */

        BX   R0 /* Jump too */

You need to become a chameleon and not just blind copy everything.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AP_040
AP_040Author
Senior
June 28, 2019

@Community member​ This all stuff are low level so, I have not much idea about this. By the way it is still not working.