Skip to main content
David.Cheng
Associate III
Apr 18, 2019 12:52 AM UTC
Question

[rtems] when enable idle interrupt uart receive nothing

HI, ALL !

i am debugging the stm32F407 uart ON RTEMS, found that the idle interrupt will effect the RX

have cleared the idle flag by pragma

but now i can not receive uart data, i don't know what's the error

uint32_t *USART2_SR = (uint32_t *)0x40004400;

uint32_t *USART2_DR = (uint32_t *)0x40004404;

#pragma GCC push_options

#pragma GCC optimize ("O0")

rtems_isr USART2_handler(rtems_vector_number vector)

{

   uint32_t temp = temp;

   uint32_t SR = *USART2_SR;

   if((*USART2_SR) & (1<<5))

   {

      

      //printk("into int\n");

       if(uart2_index < 100)

          uart2_buf[uart2_index++] = (uint8_t)(*USART2_DR)&0xff;

      else

           temp = *USART2_DR;

      //printk("%02X ", uart2_buf[uart2_index - 1]);

      

      

      

            

   }

   

   if((*USART2_SR) & (1<<4)) // idle

   {

      //printk("idle ");

       

       temp = (*USART2_SR);

      temp = (*USART2_DR);

       //temp = temp;

      

       uart2_rev_flag = 1;   

       //printk("fla %08X", *USART2_SR);

       

   }

   

   if((*USART2_SR) & (1<<3))

   {

       //int temp = (*USART2_DR)&0xff;

       temp = *USART2_SR;

      temp = *USART2_DR;

   }

   

   //temp = (*USART2_SR);

   //temp = (*USART2_DR);

   

}

#pragma GCC pop_options

my history mail post link https://lists.rtems.org/pipermail/users/2019-April/033147.html

This topic has been closed for replies.