Skip to main content
Associate
Apr 17, 2026 1:44 AM UTC
Solved

RTC stops at high temperature with LSE clock sourced from a crystal oscillator

Hello!
I am using a 32.768 kHz TCXO (TG-3541CE) as the LSE to count the RTC.
The MCU is an STM32L452RE.
At room temperature, the RTC operates correctly, but at high temperatures (around 50 °C), the RTC stops.
Strangely, once it has stopped, touching the MCU by finger causes the RTC to start running again.
Suspecting an issue with the TCXO, I tried a different TCXO, but the same behavior occurred.

When I added a 200 Ω damping resistor between the TCXO and the MCU, the RTC no longer stopped even when the temperature was raised to 60 °C.
This seems to have solved the problem for now, but I am concerned about whether 200 Ω is an appropriate value and whether this is truly a fundamental solution.
If you have any ideas about possible root causes or considerations, I would really appreciate your advice.

waclawek.jan
waclawek.janBest answer
Super User
May 7, 2026 8:04 AM UTC

You may have replied to a spammer - these days they regurgitate the thread through AI to have them look legit, and try to inject a fradulent link. That post has been manually reviewed and removed.

As you use an external TCXO, LSE drive strength should be irrelevant (AI-generated text will mention it as a LLM is trained to infer that from "LSE problems".)

At this point there's probably not much the public forum here can do to help you. You may want to contact ST directly, through FAE or the web support form.

JW

12 replies

mƎALLEm
ST Technical Moderator
Apr 17, 2026 10:29 AM UTC

Hello @Red_Mask and welcome to the ST community,

As you are using a crystal oscillator, try to isolate the crystal and supply it separately at 50°c, does it generate a normal output as for a room temperature? probe the output with an oscilloscope.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Red_MaskAuthor
Associate
Apr 20, 2026 2:07 AM UTC

I have confirmed that the oscillator continues to output 32.768 Hz waveform even at temperatures above 50°C.

LCE
Principal III
Apr 17, 2026 11:58 AM UTC

The RCC is set to LSE BYPASS ?

Red_MaskAuthor
Associate
Apr 20, 2026 2:08 AM UTC

Yes. I have set the RCC to LSE BYPASS.

waclawek.jan
Super User
Apr 20, 2026 10:39 AM UTC

Can you reproduce the problem at a "known good" board such as Nucleo?

JW

Red_MaskAuthor
Associate
Apr 20, 2026 11:57 PM UTC

OK! I will try it.

Red_MaskAuthor
Associate
Apr 27, 2026 2:39 AM UTC
I checked whether the problem occurs on a NUCLEO board.
As a result, we confirmed that the issue does not occur on a NUCLEO board.
After that, we found that even when setting the MCU (STM32L452RE) on our own board to the LSI and increasing the temperature, the RTC does not stop.
Given this, is it possible that an issue with the PCB layout or routing could cause the RTC driven by the LSE to stop?
Red_MaskAuthor
Associate
May 7, 2026 4:31 AM UTC

Thank you for your response!

I would appreciate it if you could let me know if there are any precautions to take regarding the STM32 LSE drive configuration.
Also, regarding the open link — I can’t seem to access the discussion page when I click it. Could you please send me the link again?

waclawek.jan
waclawek.janBest answer
Super User
May 7, 2026 8:04 AM UTC

You may have replied to a spammer - these days they regurgitate the thread through AI to have them look legit, and try to inject a fradulent link. That post has been manually reviewed and removed.

As you use an external TCXO, LSE drive strength should be irrelevant (AI-generated text will mention it as a LLM is trained to infer that from "LSE problems".)

At this point there's probably not much the public forum here can do to help you. You may want to contact ST directly, through FAE or the web support form.

JW