Skip to main content
p__it
Associate II
July 23, 2009
Question

RTC Prescaler wont work

  • July 23, 2009
  • 4 replies
  • 1095 views
Posted on July 23, 2009 at 05:08

RTC Prescaler wont work

    This topic has been closed for replies.

    4 replies

    p__it
    p__itAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Hello,

    i have a Problem configuring the RTC prescaler.

    This is my code:

    // -----------------------------

    // Real Time Clock konfiguration

    // -----------------------------

    void RTC_Configuration (void)

    {

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_BKP | RCC_APB1Periph_PWR, ENABLE); // Enable PWR and BKP clocks

    PWR_BackupAccessCmd(ENABLE); // Allow access to Backup Registers

    BKP_DeInit(); // Reset Backup Domain

    RCC_LSEConfig(RCC_LSE_ON);

    while (RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET); // Wait till LSE is ready

    RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); // Select LSE as RTC Clock Source

    RCC_RTCCLKCmd(ENABLE); // Enable RTC Clock

    RTC_WaitForSynchro(); // Wait for RTC registers synchronization

    RTC_WaitForLastTask(); // Wait until last write operation on RTC registers has finished

    RTC_ITConfig(RTC_IT_SEC, ENABLE); // Enable the RTC Second

    RTC_WaitForLastTask(); // Wait until last write operation on RTC registers has finishe

    // Set RTC prescaler: set RTC period to 1sec

    RTC_SetPrescaler(32767); // RTC period = RTCCLK/RTC_PR = (32.768 KHz)/(32767+1)

    RTC_WaitForLastTask(); // Wait until last write operation on RTC registers has finished

    }

    It doesnt matter which value i give the RTC_SetPrescaler function (32767 or 2 oder 16000) the Interrupt period is allways 1.6ms.

    I am using an external 32,768kHz Quartz.

    What am i doing wrong or is there missing something?

    Thanks

    p__it
    p__itAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    I found my mistake.

    I forgot to clear the RTC Second Flag in the RTC Interrupt.

    p__it
    p__itAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Thanks,

    but i didnt help.

    domen2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Try enabling RTC second interrupt after setting the prescaler.

    Also, I have

    RTC_WaitForLastTask();

    RTC_SetCounter(0);

    after set prescaler, the rest is the same.